<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic When the NFC_CSx signals are activated ? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-the-NFC-CSx-signals-are-activated/m-p/571505#M34139</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I would like to interface an array of NAND Flash Memories to an MK60F.... which has NFC interface, provided with two NFC_CSx signals. I would need more than two of them ( at least 4 )... and I am unable to find out neither the condition under which these two NFC_CSx signals are activated, nor the way I could generate more chip select signals. Could someone help me, please ? Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Aug 2016 17:18:33 GMT</pubDate>
    <dc:creator>tiborsomogyi</dc:creator>
    <dc:date>2016-08-29T17:18:33Z</dc:date>
    <item>
      <title>When the NFC_CSx signals are activated ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-the-NFC-CSx-signals-are-activated/m-p/571505#M34139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I would like to interface an array of NAND Flash Memories to an MK60F.... which has NFC interface, provided with two NFC_CSx signals. I would need more than two of them ( at least 4 )... and I am unable to find out neither the condition under which these two NFC_CSx signals are activated, nor the way I could generate more chip select signals. Could someone help me, please ? Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 17:18:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-the-NFC-CSx-signals-are-activated/m-p/571505#M34139</guid>
      <dc:creator>tiborsomogyi</dc:creator>
      <dc:date>2016-08-29T17:18:33Z</dc:date>
    </item>
    <item>
      <title>Re: When the NFC_CSx signals are activated ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-the-NFC-CSx-signals-are-activated/m-p/571506#M34140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no way to get current activated NFC_CEx signal from NFC register.&lt;/P&gt;&lt;P&gt;If customer could consider to use Flexbus module to extend external memory?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2016 06:00:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-the-NFC-CSx-signals-are-activated/m-p/571506#M34140</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-08-31T06:00:02Z</dc:date>
    </item>
  </channel>
</rss>