<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FDRM-K82F and J-Link probe in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568771#M34041</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to successfully connect to my FRDM-K82F board via my J-Link probe via J19 by removing J6 and J7 jumpers.&amp;nbsp; Since J19 is not a keyed header, please make sure that you have the proper orientation for pin 1 and that your Cortex M Adapter is not offset.&amp;nbsp; As the pins are very small, it is quite easy to do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my output below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2744i631136A9D78FE110/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, just to make sure, you are able to communicate to the MCU using the J-Link OpenSDA App with the USB Micro cable connected to J5?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Aug 2016 23:13:24 GMT</pubDate>
    <dc:creator>carlos_chavez</dc:creator>
    <dc:date>2016-08-29T23:13:24Z</dc:date>
    <item>
      <title>FDRM-K82F and J-Link probe</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568768#M34038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ALl,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to connect J-Link probe to J19 on FDRM-K82F board, so far I cannot connect, my probe is working since i can connect to K20 MCU on same board. &amp;nbsp;I remove jumpers J6 and J7 as &amp;nbsp;J17 as well, As a desperate I also remove J8 but it cannot connect after all. I am powering using USB port (not Open SDA port).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the output for K20 sucessful connection&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;XXX:~$ JLinkExe -device MK20FX512xxx12&lt;BR /&gt;SEGGER J-Link Commander V5.12g (Compiled May 27 2016 17:03:43)&lt;BR /&gt;DLL version V5.12g, compiled May 27 2016 17:03:38&lt;/P&gt;&lt;P&gt;Connecting to J-Link via USB...O.K.&lt;BR /&gt;Firmware: J-Link V9 compiled Apr 22 2016 11:47:06&lt;BR /&gt;Hardware version: V9.40&lt;BR /&gt;S/N: 269401007&lt;BR /&gt;License(s): FlashBP, GDB&lt;BR /&gt;OEM: SEGGER-EDU&lt;BR /&gt;VTref = 3.304V&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Type "connect" to establish a target connection, '?' for help&lt;BR /&gt;J-Link&amp;gt;connect&lt;BR /&gt;Please specify target interface:&lt;BR /&gt; J) JTAG (Default)&lt;BR /&gt; S) SWD&lt;BR /&gt;TIF&amp;gt;S&lt;BR /&gt;Specify target interface speed [kHz]. &amp;lt;Default&amp;gt;: 4000 kHz&lt;BR /&gt;Speed&amp;gt;&lt;BR /&gt;Device "MK20FX512XXX12" selected.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Found SWD-DP with ID 0x2BA01477&lt;BR /&gt;Found SWD-DP with ID 0x2BA01477&lt;BR /&gt;Found Cortex-M4 r0p1, Little endian.&lt;BR /&gt;FPUnit: 6 code (BP) slots and 2 literal slots&lt;BR /&gt;CoreSight components:&lt;BR /&gt;ROMTbl 0 @ E00FF000&lt;BR /&gt;ROMTbl 0 [0]: FFF0F000, CID: B105E00D, PID: 000BB000 SCS&lt;BR /&gt;ROMTbl 0 [1]: FFF02000, CID: B105E00D, PID: 003BB002 DWT&lt;BR /&gt;ROMTbl 0 [2]: FFF03000, CID: B105E00D, PID: 002BB003 FPB&lt;BR /&gt;ROMTbl 0 [3]: FFF01000, CID: B105E00D, PID: 003BB001 ITM&lt;BR /&gt;ROMTbl 0 [4]: FFF41000, CID: B105900D, PID: 000BB9A1 TPIU&lt;BR /&gt;Cortex-M4 identified.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and for K82F&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;XXX:~$ JLinkExe -device MK82FN256xxx15&lt;BR /&gt;SEGGER J-Link Commander V5.12g (Compiled May 27 2016 17:03:43)&lt;BR /&gt;DLL version V5.12g, compiled May 27 2016 17:03:38&lt;/P&gt;&lt;P&gt;Connecting to J-Link via USB...O.K.&lt;BR /&gt;Firmware: J-Link V9 compiled Apr 22 2016 11:47:06&lt;BR /&gt;Hardware version: V9.40&lt;BR /&gt;S/N: 269401007&lt;BR /&gt;License(s): FlashBP, GDB&lt;BR /&gt;OEM: SEGGER-EDU&lt;BR /&gt;VTref = 3.296V&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Type "connect" to establish a target connection, '?' for help&lt;BR /&gt;J-Link&amp;gt;connect&lt;BR /&gt;Please specify target interface:&lt;BR /&gt; J) JTAG (Default)&lt;BR /&gt; S) SWD&lt;BR /&gt;TIF&amp;gt;S&lt;BR /&gt;Specify target interface speed [kHz]. &amp;lt;Default&amp;gt;: 4000 kHz&lt;BR /&gt;Speed&amp;gt;&lt;BR /&gt;Device "MK82FN256XXX15" selected.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Can not connect to target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I missing something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would appreciate any comments.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for reading,&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Aug 2016 23:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568768#M34038</guid>
      <dc:creator>mhanuel</dc:creator>
      <dc:date>2016-08-28T23:36:00Z</dc:date>
    </item>
    <item>
      <title>Re: FDRM-K82F and J-Link probe</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568769#M34039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I am not sure which USB port you used for the power. The OpenSDA is powered by P5V_SDA with J5 USB port; If you power the board with J11 USB port, which will not provide power to OpenSDA, but only the K82 chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One another thing, did you update the OpenSDA firmware? I would recommend customer to update FRDM-K82 board OpenSDA firmware to J-Link. Customer could find and download Segger J-Link firmware from:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.segger.com/opensda.html" title="https://www.segger.com/opensda.html"&gt;SEGGER - The Embedded Experts - OpenSDA / OpenSDA V2&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 08:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568769#M34039</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-08-29T08:57:33Z</dc:date>
    </item>
    <item>
      <title>Re: FDRM-K82F and J-Link probe</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568770#M34040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Gang Li,&lt;/P&gt;&lt;P&gt;I am aware of the power supply condition you mention, I actually not interested in powering the openSDA circuitry since my willing is to debug using external J-Link probe, I need to debug the K82F only.&lt;/P&gt;&lt;P&gt;I know is getting power since it's sense by probe as shown on console output.&lt;/P&gt;&lt;P&gt;I already was using the latest J-Link firmware under openSDA, but I am willing to change to external debugger since I have more control.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I already remove J6 and J7, also I cut trace of J8 and J17. Still cannot connect. It may be a board issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your comments,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 15:44:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568770#M34040</guid>
      <dc:creator>mhanuel</dc:creator>
      <dc:date>2016-08-29T15:44:16Z</dc:date>
    </item>
    <item>
      <title>Re: FDRM-K82F and J-Link probe</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568771#M34041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to successfully connect to my FRDM-K82F board via my J-Link probe via J19 by removing J6 and J7 jumpers.&amp;nbsp; Since J19 is not a keyed header, please make sure that you have the proper orientation for pin 1 and that your Cortex M Adapter is not offset.&amp;nbsp; As the pins are very small, it is quite easy to do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my output below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2744i631136A9D78FE110/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, just to make sure, you are able to communicate to the MCU using the J-Link OpenSDA App with the USB Micro cable connected to J5?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 23:13:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568771#M34041</guid>
      <dc:creator>carlos_chavez</dc:creator>
      <dc:date>2016-08-29T23:13:24Z</dc:date>
    </item>
    <item>
      <title>Re: FDRM-K82F and J-Link probe</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568772#M34042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I install J17 and now it works. Section 3.2.1 of User Guide is kind of confusing since I thought I have to cut the trace, with that jumper in place now it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please let me know the correct way to interpret that section?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Aug 2016 03:17:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568772#M34042</guid>
      <dc:creator>mhanuel</dc:creator>
      <dc:date>2016-08-30T03:17:18Z</dc:date>
    </item>
    <item>
      <title>Re: FDRM-K82F and J-Link probe</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568773#M34043</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel,&lt;/P&gt;&lt;P&gt;&amp;nbsp; The second part of 3.2.1&amp;nbsp;is describing an additional feature of the Freedom board where you can use your FRDM-K82F to program another board. That however is an atypical use-case, and for normal board operation it's assumed that J17 wouldn't be touched nor that trace cut. You need that connection&amp;nbsp;for the SWD_CLK signal to get to the K82 device to debug.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Anthony&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Aug 2016 16:28:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FDRM-K82F-and-J-Link-probe/m-p/568773#M34043</guid>
      <dc:creator>anthony_huereca</dc:creator>
      <dc:date>2016-08-30T16:28:57Z</dc:date>
    </item>
  </channel>
</rss>