<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Problem While flashing custom PCB using OSBDM JTAG K53N512 in IAR</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-While-flashing-custom-PCB-using-OSBDM-JTAG-K53N512-in/m-p/566483#M33987</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'd highly recommend to cut out the Pin 4 (TCK/EZP_CLK) with PTA0 which can effectively isolate the on-board MCU from the OSJTAG debug interface.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Aug 2016 02:16:37 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-08-02T02:16:37Z</dc:date>
    <item>
      <title>Problem While flashing custom PCB using OSBDM JTAG K53N512 in IAR</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-While-flashing-custom-PCB-using-OSBDM-JTAG-K53N512-in/m-p/566482#M33986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; We trying to flash Bin file into the custom PCB made similar to TWR K53N512,we are using the OSBDM JTAG mechanism to flash the bin file into the custom board using TWR K53N512.&lt;BR /&gt;There is 20 pin connector named cortex Debug which we have interfaced with our custom PCB.But when we try to flash the code&amp;nbsp; using OSBDM JTAG , it shows the below error attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope for a better solution for NXP community..Since it helped me in every problem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jul 2016 05:42:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-While-flashing-custom-PCB-using-OSBDM-JTAG-K53N512-in/m-p/566482#M33986</guid>
      <dc:creator>communitycommun</dc:creator>
      <dc:date>2016-07-13T05:42:21Z</dc:date>
    </item>
    <item>
      <title>Re: Problem While flashing custom PCB using OSBDM JTAG K53N512 in IAR</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-While-flashing-custom-PCB-using-OSBDM-JTAG-K53N512-in/m-p/566483#M33987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'd highly recommend to cut out the Pin 4 (TCK/EZP_CLK) with PTA0 which can effectively isolate the on-board MCU from the OSJTAG debug interface.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2016 02:16:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-While-flashing-custom-PCB-using-OSBDM-JTAG-K53N512-in/m-p/566483#M33987</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-08-02T02:16:37Z</dc:date>
    </item>
  </channel>
</rss>