<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is P-flash swap feature(Systems using flash memory swap) available in K20P100M72SF1 ? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-P-flash-swap-feature-Systems-using-flash-memory-swap/m-p/558883#M33784</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to support Robust Firmware upgrade using this feature, which K20 shall i select? &lt;/P&gt;&lt;P&gt;I read from product documentation, that 100MHZ variant supports this swap feature, its part &lt;/P&gt;&lt;P&gt;K20P100M100SF2V2&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;Am i correct?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jul 2016 07:20:26 GMT</pubDate>
    <dc:creator>sudhanshubhutan</dc:creator>
    <dc:date>2016-07-12T07:20:26Z</dc:date>
    <item>
      <title>Is P-flash swap feature(Systems using flash memory swap) available in K20P100M72SF1 ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-P-flash-swap-feature-Systems-using-flash-memory-swap/m-p/558883#M33784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to support Robust Firmware upgrade using this feature, which K20 shall i select? &lt;/P&gt;&lt;P&gt;I read from product documentation, that 100MHZ variant supports this swap feature, its part &lt;/P&gt;&lt;P&gt;K20P100M100SF2V2&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;Am i correct?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 07:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-P-flash-swap-feature-Systems-using-flash-memory-swap/m-p/558883#M33784</guid>
      <dc:creator>sudhanshubhutan</dc:creator>
      <dc:date>2016-07-12T07:20:26Z</dc:date>
    </item>
    <item>
      <title>Re: Is P-flash swap feature(Systems using flash memory swap) available in K20P100M72SF1 ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-P-flash-swap-feature-Systems-using-flash-memory-swap/m-p/558884#M33785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sudhanshu Bhutani:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just to clarify, you mentioned datasheet document numbers and not device part numbers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About P-Flash swap:&lt;/P&gt;&lt;P&gt;- The existing K20_72 MHz parts do not have such feature.&lt;/P&gt;&lt;P&gt;- In the K20_100 MHz range the parts without FlexNVM memory have P-Flash swap feature, so you are looking for &lt;STRONG&gt;MK20DN512xxx10&lt;/STRONG&gt; part numbers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2016 20:08:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-P-flash-swap-feature-Systems-using-flash-memory-swap/m-p/558884#M33785</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-07-14T20:08:21Z</dc:date>
    </item>
  </channel>
</rss>