<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: CPU interrupt: Hard fault</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CPU-interrupt-Hard-fault/m-p/558375#M33776</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'd highly recommend you to choose the USB demos which is from the Kinetis SDK, and the most updated USB stack also integrates into the Kinetis SDK.&lt;/P&gt;&lt;P&gt;Regrading to the USB stack 4.1.1, the updates have been halted, as it has none of teams to cover it now.&lt;/P&gt;&lt;P&gt;Please refer to the thread below to install the Kinetis SDK 2.0&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="11234" data-containertype="14" data-content-finding="Community" data-objectid="329744" data-objecttype="102" href="https://community.nxp.com/docs/DOC-329744"&gt;How to: install KSDK 2.0&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Aug 2016 01:20:37 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-08-02T01:20:37Z</dc:date>
    <item>
      <title>CPU interrupt: Hard fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CPU-interrupt-Hard-fault/m-p/558374#M33775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on a tower board for MK60DN512VMD10. I have imported an example project from Freescale USB Stack v4.1.1. During debugging, I get a CPU interrupt. I would like to know how to debug this issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Aug 2016 13:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CPU-interrupt-Hard-fault/m-p/558374#M33775</guid>
      <dc:creator>kirantujare</dc:creator>
      <dc:date>2016-08-01T13:26:44Z</dc:date>
    </item>
    <item>
      <title>Re: CPU interrupt: Hard fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CPU-interrupt-Hard-fault/m-p/558375#M33776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'd highly recommend you to choose the USB demos which is from the Kinetis SDK, and the most updated USB stack also integrates into the Kinetis SDK.&lt;/P&gt;&lt;P&gt;Regrading to the USB stack 4.1.1, the updates have been halted, as it has none of teams to cover it now.&lt;/P&gt;&lt;P&gt;Please refer to the thread below to install the Kinetis SDK 2.0&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="11234" data-containertype="14" data-content-finding="Community" data-objectid="329744" data-objecttype="102" href="https://community.nxp.com/docs/DOC-329744"&gt;How to: install KSDK 2.0&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2016 01:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CPU-interrupt-Hard-fault/m-p/558375#M33776</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-08-02T01:20:37Z</dc:date>
    </item>
    <item>
      <title>Re: CPU interrupt: Hard fault</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CPU-interrupt-Hard-fault/m-p/558376#M33777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremy,&lt;BR /&gt;My entire project code was written in CodeWarrior so I need to add USB feature in CodeWarrior. Please let me know if you could provide me some help here &lt;A href="https://community.nxp.com/thread/432104"&gt;USB CDC DEVICE&lt;/A&gt; &lt;BR /&gt;I would appreciate it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;BR /&gt;Kiran Tujare&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Aug 2016 15:59:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CPU-interrupt-Hard-fault/m-p/558376#M33777</guid>
      <dc:creator>kirantujare</dc:creator>
      <dc:date>2016-08-08T15:59:44Z</dc:date>
    </item>
  </channel>
</rss>