<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Using the ID acceptance filter MSCAN KEA128?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/557735#M33762</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to understand how the id acceptance filter for MSCAN works in KEA128, does any one have an idea of how it works?, how the&amp;nbsp; CANIDAR0-CANIDAR3, CANIDMR0-CANIDMR3 registers have to be configured? which logical operator is used where comparing the registers with the id read (or,and,etc)? which result will remain after passing all the filters for an id to be accepted?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read section 32.4.5 Identifier acceptance filter, but I don't figure it out how it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Emilio Moyers&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 31 Jul 2016 16:39:22 GMT</pubDate>
    <dc:creator>emilioaronmoyer</dc:creator>
    <dc:date>2016-07-31T16:39:22Z</dc:date>
    <item>
      <title>Using the ID acceptance filter MSCAN KEA128?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/557735#M33762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to understand how the id acceptance filter for MSCAN works in KEA128, does any one have an idea of how it works?, how the&amp;nbsp; CANIDAR0-CANIDAR3, CANIDMR0-CANIDMR3 registers have to be configured? which logical operator is used where comparing the registers with the id read (or,and,etc)? which result will remain after passing all the filters for an id to be accepted?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read section 32.4.5 Identifier acceptance filter, but I don't figure it out how it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Emilio Moyers&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 31 Jul 2016 16:39:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/557735#M33762</guid>
      <dc:creator>emilioaronmoyer</dc:creator>
      <dc:date>2016-07-31T16:39:22Z</dc:date>
    </item>
    <item>
      <title>Re: Using the ID acceptance filter MSCAN KEA128?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/557736#M33763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Emilio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you have read section&amp;nbsp; 32.4.5 Identifier acceptance filter in the RM of KEA128, the MACAN receiver is a 5 stage FIFO instead of separate message buffers, there is only one address space for the receiver FIFO, the actual message ID which is received by MSCAN is saved in MSCAN_REIDR0~3 for 29 bits extended ID and MSCAN_REIDR0~1 for 11 bits standard ID.&lt;/P&gt;&lt;P&gt;Regarding the acceptance of filter, there are two bank: fisrt bank and second bank. &lt;/P&gt;&lt;P&gt;The first bank includes the following registers:&lt;/P&gt;&lt;P&gt;MSCAN_CANIDAR0~3&lt;/P&gt;&lt;P&gt;MSCAN_CANIDMR0~3&lt;/P&gt;&lt;P&gt;The second bank includes the following registers:&lt;/P&gt;&lt;P&gt;MSCAN_CANIDAR4~7&lt;/P&gt;&lt;P&gt;MSCAN_CANIDMR4~7&lt;/P&gt;&lt;P&gt;The IDAM bits in MSCAN_CANIDAC define the filter pattern, I copy it here:&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;Identifier Acceptance Mode&lt;/P&gt;&lt;P&gt;The CPU sets these flags to define the identifier acceptance filter organization.&lt;/P&gt;&lt;P&gt;In filter closed mode, no message is accepted such that the foreground buffer is never reloaded.&lt;/P&gt;&lt;P&gt;00 Two 32-bit acceptance filters.&lt;/P&gt;&lt;P&gt;01 Four 16-bit acceptance filters.&lt;/P&gt;&lt;P&gt;10 Eight 8-bit acceptance filters.&lt;/P&gt;&lt;P&gt;11 Filter closed.&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;Assume that you set the IDAM bits as 00 in binary, the "Two 32-bit acceptance filters" pattern filter is used because there are two bank.&lt;/P&gt;&lt;P&gt;Assume you use 11 bits standard pattern, I think you can use the following pattern for the first/second bank:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1444iA6C4FA28FCA01C7F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you use 29 bits extended ID, you can use the following pattern for first/second bank:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1512i29D3A2502EBD3D86/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I copy the figure from RM of MC56F80x, they are all use MSCAN, the patten is the same.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2016 04:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/557736#M33763</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-08-02T04:19:10Z</dc:date>
    </item>
    <item>
      <title>Re: Using the ID acceptance filter MSCAN KEA128?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/557737#M33764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example if I only what to pass the messages with the ID 0x55 (standard id), waht do I need to put in the first bank registers ( &lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;MSCAN_CANIDAR0~3,MSCAN_CANIDMR0~3)?&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Regards,&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Emilio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2016 17:10:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/557737#M33764</guid>
      <dc:creator>emilioaronmoyer</dc:creator>
      <dc:date>2016-08-02T17:10:43Z</dc:date>
    </item>
    <item>
      <title>Re: Using the ID acceptance filter MSCAN KEA128?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/557738#M33765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Emilio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MSCAN_IDARx register and the MSCAN_RSIDRx register match each other, if you set the received ID as 0x55(the ID bits is 000 0101 0101), and set the IDAM bits as 00, you can set as following:&lt;/P&gt;&lt;P&gt;MSCAN_CANIDAR0=0x0C; //it include ID10~3&lt;/P&gt;&lt;P&gt;MSCAN_CANIDAR1=0xC0&amp;nbsp; //it includes ID2~0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can set the MSCAN_CANIDMR0=0xFF; MSCAN_CANIDMR1=0xF8;&lt;/P&gt;&lt;P&gt;It is okay.&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Aug 2016 02:54:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/557738#M33765</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-08-03T02:54:40Z</dc:date>
    </item>
    <item>
      <title>Re: Using the ID acceptance filter MSCAN KEA128?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/557739#M33766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; font-size: 14px;"&gt;Xiangjun, with this configuration:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;MSCAN_CANIDAR0=0x0C; //it include ID10~3&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;MSCAN_CANIDAR1=0xC0&amp;nbsp; //it includes ID2~0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;MSCAN_CANIDMR0=0xFF; MSCAN_CANIDMR1=0xF8;&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;¿which id wold pass the filter? I dont understad the logical operation. In this example:&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;id&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0000 1010 101&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;dar&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0000 1100 1100&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;dmr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1111&amp;nbsp; 1111&amp;nbsp; 1111&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;i dont understand, why id 0x55 pass the filter?&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Regards,&lt;/P&gt;&lt;P style="font-size: 14px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Julian echeverry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 05:09:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/557739#M33766</guid>
      <dc:creator>julianmauricioe</dc:creator>
      <dc:date>2016-08-10T05:09:34Z</dc:date>
    </item>
    <item>
      <title>Re: Using the ID acceptance filter MSCAN KEA128?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/1327190#M61312</link>
      <description>&lt;P&gt;Hii&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Can you explain the logic behind this masking, its not clear please provide explanation with other examples&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Sat, 21 Aug 2021 12:51:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-the-ID-acceptance-filter-MSCAN-KEA128/m-p/1327190#M61312</guid>
      <dc:creator>Arun5</dc:creator>
      <dc:date>2021-08-21T12:51:25Z</dc:date>
    </item>
  </channel>
</rss>