<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Uploading program to FRDM-K82f using command line or drag drop</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Uploading-program-to-FRDM-K82f-using-command-line-or-drag-drop/m-p/555750#M33682</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to upload demo apps on my FRDM-K82f board. The default bootloader was of mbed, in which I was able to drag and drop the files to program. After that I uploaded OpenSDA bootloader v2.1 on the board. I've followed the steps mentioned in user guide and can successfully run demo apps using GDBServer method. But when I try to drag and drop files now, the board doesn't program.&lt;/P&gt;&lt;P&gt;Also is there any utility to program the board using command line or if you can mention the commands that can be used for programming through JLinkExe that'd be great. I am using SDK with GCC on Linux.&lt;/P&gt;&lt;P&gt;Thanks in advance for help :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 09 Jul 2016 13:46:13 GMT</pubDate>
    <dc:creator>lalit0611</dc:creator>
    <dc:date>2016-07-09T13:46:13Z</dc:date>
    <item>
      <title>Uploading program to FRDM-K82f using command line or drag drop</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Uploading-program-to-FRDM-K82f-using-command-line-or-drag-drop/m-p/555750#M33682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to upload demo apps on my FRDM-K82f board. The default bootloader was of mbed, in which I was able to drag and drop the files to program. After that I uploaded OpenSDA bootloader v2.1 on the board. I've followed the steps mentioned in user guide and can successfully run demo apps using GDBServer method. But when I try to drag and drop files now, the board doesn't program.&lt;/P&gt;&lt;P&gt;Also is there any utility to program the board using command line or if you can mention the commands that can be used for programming through JLinkExe that'd be great. I am using SDK with GCC on Linux.&lt;/P&gt;&lt;P&gt;Thanks in advance for help :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jul 2016 13:46:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Uploading-program-to-FRDM-K82f-using-command-line-or-drag-drop/m-p/555750#M33682</guid>
      <dc:creator>lalit0611</dc:creator>
      <dc:date>2016-07-09T13:46:13Z</dc:date>
    </item>
    <item>
      <title>Re: Uploading program to FRDM-K82f using command line or drag drop</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Uploading-program-to-FRDM-K82f-using-command-line-or-drag-drop/m-p/555751#M33683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The bootloader itself does not have target device programming (except the K20). Have a look at the latest Segger firmware which includes virtual MSD and programming: &lt;A href="https://mcuoneclipse.com/2016/06/19/segger-opensda-firmware-with-virtual-msd/" title="https://mcuoneclipse.com/2016/06/19/segger-opensda-firmware-with-virtual-msd/"&gt;https://mcuoneclipse.com/2016/06/19/segger-opensda-firmware-with-virtual-msd/&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And here is a simple script how to program a device: &lt;A href="https://mcuoneclipse.com/2016/06/26/how-to-recover-the-opensda-v2-x-bootloader/" title="https://mcuoneclipse.com/2016/06/26/how-to-recover-the-opensda-v2-x-bootloader/"&gt;https://mcuoneclipse.com/2016/06/26/how-to-recover-the-opensda-v2-x-bootloader/&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jul 2016 14:15:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Uploading-program-to-FRDM-K82f-using-command-line-or-drag-drop/m-p/555751#M33683</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-07-09T14:15:22Z</dc:date>
    </item>
    <item>
      <title>Re: Uploading program to FRDM-K82f using command line or drag drop</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Uploading-program-to-FRDM-K82f-using-command-line-or-drag-drop/m-p/555752#M33684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;About the first link, when I copy the file to the drive, nothing seems to happen. I've tried .hex files.&lt;/P&gt;&lt;P&gt;About the second link, JLink looks like a good way to go, I'll try that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT:&lt;/P&gt;&lt;P&gt;The problem that I've mentioned below has been resolved. It was just the wrong pin_mux files in my project. But the first problem remains.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I've installed KDS setup wizard addon to Eclipse, I'm able to build the project but when I try to debug, debugger runs but the code is not running on the board. Is there any setting that I need to change in the debug configurations. My current configuration is attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36189i448E0589D35F47CD/image-size/large?v=v2&amp;amp;px=999" title="Screenshot from 2016-07-09 23_31_37.png" alt="Screenshot from 2016-07-09 23_31_37.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36148iD7413744BB5B83EA/image-size/large?v=v2&amp;amp;px=999" title="Screenshot from 2016-07-09 23_31_53.png" alt="Screenshot from 2016-07-09 23_31_53.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jul 2016 18:04:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Uploading-program-to-FRDM-K82f-using-command-line-or-drag-drop/m-p/555752#M33684</guid>
      <dc:creator>lalit0611</dc:creator>
      <dc:date>2016-07-09T18:04:04Z</dc:date>
    </item>
    <item>
      <title>Re: Uploading program to FRDM-K82f using command line or drag drop</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Uploading-program-to-FRDM-K82f-using-command-line-or-drag-drop/m-p/555753#M33685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Your settings look ok.&lt;/P&gt;&lt;P&gt;After your edit, I'm not sure what your problem is?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jul 2016 18:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Uploading-program-to-FRDM-K82f-using-command-line-or-drag-drop/m-p/555753#M33685</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-07-09T18:37:16Z</dc:date>
    </item>
    <item>
      <title>Re: Uploading program to FRDM-K82f using command line or drag drop</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Uploading-program-to-FRDM-K82f-using-command-line-or-drag-drop/m-p/555754#M33686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem is that drag n drop still doesn't work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jul 2016 18:53:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Uploading-program-to-FRDM-K82f-using-command-line-or-drag-drop/m-p/555754#M33686</guid>
      <dc:creator>lalit0611</dc:creator>
      <dc:date>2016-07-09T18:53:30Z</dc:date>
    </item>
  </channel>
</rss>