<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KL25Z not recognized</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555438#M33668</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I follow the instruction. The problem is that when I hold reset and plug the board in, the on board LED will flash fast 7-8 times and pause for 1 sec. &amp;nbsp;Even the bootloader drive shows up, and I drag files to it, it does not seems to work properly. &amp;nbsp;When I power down and back up in normal mode, the board could not be recognized. I tried to update the bootloader app to v1.11 and failed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any idea what does the fast blinking LED indicates? &amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Aug 2016 14:31:10 GMT</pubDate>
    <dc:creator>rebeccachang</dc:creator>
    <dc:date>2016-08-24T14:31:10Z</dc:date>
    <item>
      <title>KL25Z not recognized</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555434#M33664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a KL25Z board not recognized by the Windows 7 64-bit PC. &amp;nbsp;I can get into the bootloader mode to update FW, but after power cycle the board was not detectable by the PC (no mbed drive mounted).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I had the board for a while and it was functioning fine until today. &amp;nbsp;It started out that the board was recognizable and I can see the mbed drive. &amp;nbsp;However&amp;nbsp;my program (.bin) was not executing correctly. &amp;nbsp;So I reloaded FW(20140530_k20dx128_kl25z_if_opensda.s19) via the BOOTLOADER mode. &amp;nbsp;After the FW update,&amp;nbsp;the board became undetectable by the PC. &amp;nbsp;I can still get into the bootloader mode, the on board LED will flash fast 7-8 times then pause for 1 sec. I tried the same process (FW reload) using&amp;nbsp;another KL25Z (again one that used to function well) and getting the same result (board nolonger recognizable). &amp;nbsp;I tried another Windows 7 machine with no luck. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any one had similar experience? &amp;nbsp;Please help! &amp;nbsp;Thanks in advance. &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 06:56:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555434#M33664</guid>
      <dc:creator>rebeccachang</dc:creator>
      <dc:date>2016-08-24T06:56:21Z</dc:date>
    </item>
    <item>
      <title>Re: KL25Z not recognized</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555435#M33665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rebecca,&lt;/P&gt;&lt;P&gt;see &lt;A class="link-titled" href="https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-freedom-board-firmware/" title="https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-freedom-board-firmware/"&gt;https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-freedom-board-firmware/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Make sure you extract the firmware file from the archive. Use the DOS shell/cmd copy command to copy the file as some explorer extensions can cause problems. Additionally you might turn off any firewalls/virus scanners as they could cause issues during the copy.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 07:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555435#M33665</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-08-24T07:29:58Z</dc:date>
    </item>
    <item>
      <title>Re: KL25Z not recognized</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555436#M33666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric, thanks for the quick reply. &amp;nbsp;I have tried the method you referenced to. &amp;nbsp;When I pressed the reset button while powering on the board to get to the bootloader mode, the on board LED would flash very fast for 7-8 times then pause 1 sec. &amp;nbsp;According to the instruction,the LED should blink at 1hz rate. &amp;nbsp;If I plug the board to the PC without pressing the reset button, the board would not be recognized and the LED stays off. &amp;nbsp;Any idea what's the issue here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW, the PEmicro site is down. &amp;nbsp;anywhere else I can download the latest bootloader? &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 13:53:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555436#M33666</guid>
      <dc:creator>rebeccachang</dc:creator>
      <dc:date>2016-08-24T13:53:15Z</dc:date>
    </item>
    <item>
      <title>Re: KL25Z not recognized</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555437#M33667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric, the PEmicro site if back up now. &amp;nbsp;I was able to download the latest Bootloader app. &amp;nbsp;But I still stuck at when I hold the RESET while plug into the board to go into bootloader mode, the LED blinks fast 7-8 times then pause. Even the boothloader drive shows up, and I can drag files to it. &amp;nbsp;It doesn't seem to work. &amp;nbsp;When I power off and on in normal mode, the board will not be recognized. &amp;nbsp;What does it mean when the LED blink fast and pause? &amp;nbsp;I even reinstall the driver with no difference.&amp;nbsp;&lt;/P&gt;&lt;P&gt;THanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 14:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555437#M33667</guid>
      <dc:creator>rebeccachang</dc:creator>
      <dc:date>2016-08-24T14:27:54Z</dc:date>
    </item>
    <item>
      <title>Re: KL25Z not recognized</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555438#M33668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I follow the instruction. The problem is that when I hold reset and plug the board in, the on board LED will flash fast 7-8 times and pause for 1 sec. &amp;nbsp;Even the bootloader drive shows up, and I drag files to it, it does not seems to work properly. &amp;nbsp;When I power down and back up in normal mode, the board could not be recognized. I tried to update the bootloader app to v1.11 and failed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any idea what does the fast blinking LED indicates? &amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 14:31:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555438#M33668</guid>
      <dc:creator>rebeccachang</dc:creator>
      <dc:date>2016-08-24T14:31:10Z</dc:date>
    </item>
    <item>
      <title>Re: KL25Z not recognized</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555439#M33669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rebecca,&lt;/P&gt;&lt;P&gt;if the board flashes that way, it means it has detected an error.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/" title="https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/"&gt;https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/&lt;/A&gt; shows a list of error codes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So when you copy the firmware file, it won't flash an error code, only when you reboot the board normally?&lt;/P&gt;&lt;P&gt;Can you try with the attached one (P&amp;amp;E)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 15:13:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555439#M33669</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-08-24T15:13:55Z</dc:date>
    </item>
    <item>
      <title>Re: KL25Z not recognized</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555440#M33670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;My board symptom matches well on what you describe in the video "Bricking and unbricking opensSDA with win 8 and 10".&lt;/P&gt;&lt;P&gt;I tried to follow your solution by enable the setting of "Computer Configuration \ Administrative Templates \ Windows Components \ Search \&lt;STRONG style="color: #373737; background-color: #ffffff; border: 0px; font-weight: bold;"&gt; Do not allow locations on removable drives to be added to libraries". &amp;nbsp;&lt;/STRONG&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;The problem now is I am using Window 7 and &amp;nbsp;I don't see &amp;nbsp; "Do not allow locations on removable drives to be added to libraries" in the group policy editor. &amp;nbsp; &amp;nbsp; What should I do? &amp;nbsp; &amp;nbsp; &amp;nbsp;thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 18:24:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555440#M33670</guid>
      <dc:creator>rebeccachang</dc:creator>
      <dc:date>2016-08-24T18:24:58Z</dc:date>
    </item>
    <item>
      <title>Re: KL25Z not recognized</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555441#M33671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rebecca,&lt;/P&gt;&lt;P&gt;that setting is probably only available on Win8/10.&lt;/P&gt;&lt;P&gt;Have you:&lt;/P&gt;&lt;P&gt;- disabled any virus scanner/fire walls&lt;/P&gt;&lt;P&gt;- disabled any explorer extensions&lt;/P&gt;&lt;P&gt;- unzipped the file&lt;/P&gt;&lt;P&gt;- copied the file with the cmd.exe (command prompt)&lt;/P&gt;&lt;P&gt;?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend that you try it with another Windows 7 machine, as I think your machine has some specific settings which try to write to the device in a unexpected way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2016 05:57:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL25Z-not-recognized/m-p/555441#M33671</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-08-25T05:57:12Z</dc:date>
    </item>
  </channel>
</rss>