<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can someone tell me how to make a timer in KL27Z microcontroller so that it starts to count the seconds? Thank you in advance in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-someone-tell-me-how-to-make-a-timer-in-KL27Z-microcontroller/m-p/553095#M33612</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to make a timer in KL27Z using Kinetis development studio and have no idea how to make it. Could someone help me in this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Aug 2016 10:00:56 GMT</pubDate>
    <dc:creator>vivekgarg</dc:creator>
    <dc:date>2016-08-24T10:00:56Z</dc:date>
    <item>
      <title>Can someone tell me how to make a timer in KL27Z microcontroller so that it starts to count the seconds? Thank you in advance</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-someone-tell-me-how-to-make-a-timer-in-KL27Z-microcontroller/m-p/553095#M33612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to make a timer in KL27Z using Kinetis development studio and have no idea how to make it. Could someone help me in this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 10:00:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-someone-tell-me-how-to-make-a-timer-in-KL27Z-microcontroller/m-p/553095#M33612</guid>
      <dc:creator>vivekgarg</dc:creator>
      <dc:date>2016-08-24T10:00:56Z</dc:date>
    </item>
    <item>
      <title>Re: Can someone tell me how to make a timer in KL27Z microcontroller so that it starts to count the seconds? Thank you in advance</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-someone-tell-me-how-to-make-a-timer-in-KL27Z-microcontroller/m-p/553096#M33613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vivek.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to PIT example, which is part of &lt;A href="http://nxp.com/ksdk"&gt;KSDK&lt;/A&gt;. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PIT project is a simple demonstration program of the SDK PIT driver. It sets up the PIT&lt;BR /&gt;hardware block to trigger a periodic interrupt after every 1 second. When the PIT interrupt is triggered&lt;BR /&gt;a message a printed on the UART terminal and an LED is toggled on the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#include "fsl_debug_console.h"&lt;BR /&gt;#include "board.h"&lt;BR /&gt;#include "fsl_pit.h"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#include "pin_mux.h"&lt;BR /&gt;#include "clock_config.h"&lt;BR /&gt;/*******************************************************************************&lt;BR /&gt;&amp;nbsp;* Definitions&lt;BR /&gt;&amp;nbsp;******************************************************************************/&lt;BR /&gt;#define PIT_LED_HANDLER PIT_IRQHandler&lt;BR /&gt;#define PIT_IRQ_ID PIT_IRQn&lt;BR /&gt;/* Get source clock for PIT driver */&lt;BR /&gt;#define PIT_SOURCE_CLOCK CLOCK_GetFreq(kCLOCK_BusClk)&lt;BR /&gt;#define LED_INIT() LED_RED_INIT(LOGIC_LED_ON)&lt;BR /&gt;#define LED_TOGGLE() LED_RED_TOGGLE()&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*******************************************************************************&lt;BR /&gt;&amp;nbsp;* Prototypes&lt;BR /&gt;&amp;nbsp;******************************************************************************/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*******************************************************************************&lt;BR /&gt;&amp;nbsp;* Variables&lt;BR /&gt;&amp;nbsp;******************************************************************************/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;volatile bool pitIsrFlag = false;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*******************************************************************************&lt;BR /&gt;&amp;nbsp;* Code&lt;BR /&gt;&amp;nbsp;******************************************************************************/&lt;BR /&gt;void PIT_LED_HANDLER(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Clear interrupt flag.*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PIT_ClearStatusFlags(PIT, kPIT_Chnl_0, PIT_TFLG_TIF_MASK);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pitIsrFlag = true;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*!&lt;BR /&gt;&amp;nbsp;* @brief Main function&lt;BR /&gt;&amp;nbsp;*/&lt;BR /&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Structure of initialize PIT */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pit_config_t pitConfig;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Initialize and enable LED */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LED_INIT();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Board pin, clock, debug console init */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_InitPins();&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_BootClockRUN();&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_InitDebugConsole();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; * pitConfig.enableRunInDebug = false;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PIT_GetDefaultConfig(&amp;amp;pitConfig);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Init pit module */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PIT_Init(PIT, &amp;amp;pitConfig);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Set timer period for channel 0 */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PIT_SetTimerPeriod(PIT, kPIT_Chnl_0, USEC_TO_COUNT(1000000U, PIT_SOURCE_CLOCK));&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enable timer interrupts for channel 0 */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PIT_EnableInterrupts(PIT, kPIT_Chnl_0, kPIT_TimerInterruptEnable);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enable at the NVIC */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; EnableIRQ(PIT_IRQ_ID);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Start channel 0 */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PRINTF("\r\nStarting channel No.0 ...");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PIT_StartTimer(PIT, kPIT_Chnl_0);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (true)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Check whether occur interupt and toggle LED */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (true == pitIsrFlag)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PRINTF("\r\n Channel No.0 interrupt is occured !");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LED_TOGGLE();&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pitIsrFlag = false;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Iva&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 11:34:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-someone-tell-me-how-to-make-a-timer-in-KL27Z-microcontroller/m-p/553096#M33613</guid>
      <dc:creator>ivadorazinova</dc:creator>
      <dc:date>2016-09-13T11:34:42Z</dc:date>
    </item>
  </channel>
</rss>