<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックHigh Speed RNDIS and CDC composite (?)</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/High-Speed-RNDIS-and-CDC-composite/m-p/552624#M33597</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am wondering whether anyone has used RNDIS + CDC composite on a K61 or K70's HS USB interface?&lt;/P&gt;&lt;P&gt;The issue that I have is that I can do this on any FS USB interface since they have 16 endpoints but the K61/K70's HS USB has just 4 and this configuration essentilly needs 5:&lt;/P&gt;&lt;P&gt;- Endpoint 0 - control&lt;/P&gt;&lt;P&gt;- Endpoint 1 - RNDIS bulk IN/OUT&lt;/P&gt;&lt;P&gt;- Endpoint 2 - RNDIS interrupt&lt;/P&gt;&lt;P&gt;- Endpoint 3 - CDC bulk IN/OUT&lt;/P&gt;&lt;P&gt;- Endpoint 4 - CDC interrupt&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact the CDC interrupt endpoint is not used in practice but I don't know whether there is any way to configure so that it is not needed to satisfy the host or whether there is some other trick to get around this.&lt;/P&gt;&lt;P&gt;Any ideas (without having to move to K66 with 8 HS endpoints)???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 09 Jul 2016 20:18:32 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2016-07-09T20:18:32Z</dc:date>
    <item>
      <title>High Speed RNDIS and CDC composite (?)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/High-Speed-RNDIS-and-CDC-composite/m-p/552624#M33597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am wondering whether anyone has used RNDIS + CDC composite on a K61 or K70's HS USB interface?&lt;/P&gt;&lt;P&gt;The issue that I have is that I can do this on any FS USB interface since they have 16 endpoints but the K61/K70's HS USB has just 4 and this configuration essentilly needs 5:&lt;/P&gt;&lt;P&gt;- Endpoint 0 - control&lt;/P&gt;&lt;P&gt;- Endpoint 1 - RNDIS bulk IN/OUT&lt;/P&gt;&lt;P&gt;- Endpoint 2 - RNDIS interrupt&lt;/P&gt;&lt;P&gt;- Endpoint 3 - CDC bulk IN/OUT&lt;/P&gt;&lt;P&gt;- Endpoint 4 - CDC interrupt&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact the CDC interrupt endpoint is not used in practice but I don't know whether there is any way to configure so that it is not needed to satisfy the host or whether there is some other trick to get around this.&lt;/P&gt;&lt;P&gt;Any ideas (without having to move to K66 with 8 HS endpoints)???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jul 2016 20:18:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/High-Speed-RNDIS-and-CDC-composite/m-p/552624#M33597</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-07-09T20:18:32Z</dc:date>
    </item>
  </channel>
</rss>