<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK10: What voltage range can the analog inputs withstand?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-What-voltage-range-can-the-analog-inputs-withstand/m-p/552446#M33583</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;We have a K10 design where under certain circumstances the voltage reaching the ADC inputs can exceed the VREFH levels and would like to know if this will cause damage, cause the ADC to mis-operate, or inflict other consequences. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;There is a table on page 11 of the data sheet that indicates "analog input voltage" can only go up to Vdd + 0.3 V, but it is punctuated by a footnote. Under the footnote we read:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier; font-size: 10pt;"&gt;&amp;nbsp; "Analog pins are defined as pins that do not have an&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier; font-size: 10pt;"&gt;&amp;nbsp;&amp;nbsp; associated general purpose I/O port function."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;We aren't using any of those inputs: all our analog inputs are multiplexed with digital inputs. There is missing text in this data sheet. If I were to fill in the blank, I would assume that analog inputs that share a pin with digital inputs are digital inputs, and the same table allows them to accept up to 5.5 V, which would solve my problem. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;I hate to base my design safety on a sentence that isn't there. Has anyone found an unambiguous spec?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Jul 2016 09:34:44 GMT</pubDate>
    <dc:creator>garylynch</dc:creator>
    <dc:date>2016-07-08T09:34:44Z</dc:date>
    <item>
      <title>K10: What voltage range can the analog inputs withstand?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-What-voltage-range-can-the-analog-inputs-withstand/m-p/552446#M33583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;We have a K10 design where under certain circumstances the voltage reaching the ADC inputs can exceed the VREFH levels and would like to know if this will cause damage, cause the ADC to mis-operate, or inflict other consequences. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;There is a table on page 11 of the data sheet that indicates "analog input voltage" can only go up to Vdd + 0.3 V, but it is punctuated by a footnote. Under the footnote we read:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier; font-size: 10pt;"&gt;&amp;nbsp; "Analog pins are defined as pins that do not have an&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier new,courier; font-size: 10pt;"&gt;&amp;nbsp;&amp;nbsp; associated general purpose I/O port function."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;We aren't using any of those inputs: all our analog inputs are multiplexed with digital inputs. There is missing text in this data sheet. If I were to fill in the blank, I would assume that analog inputs that share a pin with digital inputs are digital inputs, and the same table allows them to accept up to 5.5 V, which would solve my problem. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;I hate to base my design safety on a sentence that isn't there. Has anyone found an unambiguous spec?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jul 2016 09:34:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-What-voltage-range-can-the-analog-inputs-withstand/m-p/552446#M33583</guid>
      <dc:creator>garylynch</dc:creator>
      <dc:date>2016-07-08T09:34:44Z</dc:date>
    </item>
    <item>
      <title>Re: K10: What voltage range can the analog inputs withstand?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-What-voltage-range-can-the-analog-inputs-withstand/m-p/552447#M33584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;We only recommend customer to make sure that ADC &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;input&lt;/SPAN&gt; voltage fall between &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;VREFH&lt;/SPAN&gt; and VREFL. &lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;Input&lt;/SPAN&gt; voltages between &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;VREFH&lt;/SPAN&gt; and VREFL are straight line linear conversions.&lt;SPAN style="font-size: 10pt;"&gt;If the Vin voltage value is higher than &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;VREFH&lt;/SPAN&gt; but lower than VDDA, the pin will not be damaged but measure result will be full-scale max value. Anyway, do not make Vin exceed the VDDA.( if VDDA is not same as VREFH.)&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jul 2016 09:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K10-What-voltage-range-can-the-analog-inputs-withstand/m-p/552447#M33584</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-07-13T09:12:08Z</dc:date>
    </item>
  </channel>
</rss>