<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K20 FTM , deadtimes in Combine Mode and ProcessorExpert</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-FTM-deadtimes-in-Combine-Mode-and-ProcessorExpert/m-p/208838#M3351</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I parsed that as the deadtime feature working in Combined mode, and the deadtime feature working in Complementary mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If indeed it won't work in Combined mode, it would be a lot more clear if the manual simply said:&lt;/P&gt;&lt;P&gt;"The deadtime feature should only be used in Complementary mode."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I say this because Complementary mode is a subset of Combined mode.&amp;nbsp; You can be in Combined mode without having the Complementary bit set, but you can't be in Complementary mode without having the Combined bit set.&lt;/P&gt;&lt;P&gt;Why even bring up Combined?&amp;nbsp; It just confuses the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand, having the deadtime feature working in Combined mode makes a lot of sense.&amp;nbsp; For a half-bridge with P and N type FETs,&amp;nbsp; you need to raise one type's gate to turn it off, and you need to raise the other type's gate to turn it on.&lt;/P&gt;&lt;P&gt;The documentation says both channels output the same signal in Combined mode if the COMP bit is not set.&lt;/P&gt;&lt;P&gt;So Combined will work for a complementary pair, with both pins driving the same direction, but you'll get shoot through.&amp;nbsp; So even though both pins need to go in the same direction, you'd like a delay between switching off one type and switching on the other. That is to say, deadtime.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It just seemed really unlikely to me that the engineers designing the module wouldn't be aware of this very common use case, and accomodated it.&lt;/P&gt;&lt;P&gt;But if they didn't, they didn't.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Feb 2013 18:30:14 GMT</pubDate>
    <dc:creator>timward</dc:creator>
    <dc:date>2013-02-21T18:30:14Z</dc:date>
    <item>
      <title>K20 FTM , deadtimes in Combine Mode and ProcessorExpert</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-FTM-deadtimes-in-Combine-Mode-and-ProcessorExpert/m-p/208836#M3349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The documentation for the FlexTimer says deadtimes can be used in combined mode.&lt;/P&gt;&lt;P&gt;ProcessorExpert flags an error if the combined channel isn't set to complementary when deadtime is enabled.&lt;/P&gt;&lt;P&gt;In fact, I can't find a spot in ProcessorExpert to set the length of the deadtimes.&lt;/P&gt;&lt;P&gt;Do I just need to hand code the initialization?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Dec 2012 01:39:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-FTM-deadtimes-in-Combine-Mode-and-ProcessorExpert/m-p/208836#M3349</guid>
      <dc:creator>timward</dc:creator>
      <dc:date>2012-12-15T01:39:01Z</dc:date>
    </item>
    <item>
      <title>Re: K20 FTM , deadtimes in Combine Mode and ProcessorExpert</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-FTM-deadtimes-in-Combine-Mode-and-ProcessorExpert/m-p/208837#M3350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you try to configure the combine mode and deadtime Processor Expert shows the next message:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"The Complementary mode must be enabled for deadtime insertion"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;This is because Processor Expert is based in the documentation that Freescale offers. As the Reference Manual for Kinetis products says:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38733i50FAC80DB8090273/image-size/large?v=v2&amp;amp;px=999" title="note FTM combine mode.png" alt="note FTM combine mode.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hence it is necessary to set Combine and Complementary modes to use deadtime. Different configurations are out of specification.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 19:20:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-FTM-deadtimes-in-Combine-Mode-and-ProcessorExpert/m-p/208837#M3350</guid>
      <dc:creator>adriansc</dc:creator>
      <dc:date>2013-02-15T19:20:53Z</dc:date>
    </item>
    <item>
      <title>Re: K20 FTM , deadtimes in Combine Mode and ProcessorExpert</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-FTM-deadtimes-in-Combine-Mode-and-ProcessorExpert/m-p/208838#M3351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I parsed that as the deadtime feature working in Combined mode, and the deadtime feature working in Complementary mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If indeed it won't work in Combined mode, it would be a lot more clear if the manual simply said:&lt;/P&gt;&lt;P&gt;"The deadtime feature should only be used in Complementary mode."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I say this because Complementary mode is a subset of Combined mode.&amp;nbsp; You can be in Combined mode without having the Complementary bit set, but you can't be in Complementary mode without having the Combined bit set.&lt;/P&gt;&lt;P&gt;Why even bring up Combined?&amp;nbsp; It just confuses the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand, having the deadtime feature working in Combined mode makes a lot of sense.&amp;nbsp; For a half-bridge with P and N type FETs,&amp;nbsp; you need to raise one type's gate to turn it off, and you need to raise the other type's gate to turn it on.&lt;/P&gt;&lt;P&gt;The documentation says both channels output the same signal in Combined mode if the COMP bit is not set.&lt;/P&gt;&lt;P&gt;So Combined will work for a complementary pair, with both pins driving the same direction, but you'll get shoot through.&amp;nbsp; So even though both pins need to go in the same direction, you'd like a delay between switching off one type and switching on the other. That is to say, deadtime.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It just seemed really unlikely to me that the engineers designing the module wouldn't be aware of this very common use case, and accomodated it.&lt;/P&gt;&lt;P&gt;But if they didn't, they didn't.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2013 18:30:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20-FTM-deadtimes-in-Combine-Mode-and-ProcessorExpert/m-p/208838#M3351</guid>
      <dc:creator>timward</dc:creator>
      <dc:date>2013-02-21T18:30:14Z</dc:date>
    </item>
  </channel>
</rss>