<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MK02FN Flashloader</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02FN-Flashloader/m-p/547028#M33352</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ken Roberts:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please read the response from colleague Carlos Chavez in the next thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/338502"&gt;FlashLoader on Kinetis MK02, Incorrect Peripherals, Error in Reference Manual&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The errata is already in place: &lt;A href="http://cache.nxp.com/files/32bit/doc/errata/KINETIS_K_0N36M.pdf" title="http://cache.nxp.com/files/32bit/doc/errata/KINETIS_K_0N36M.pdf"&gt;http://cache.nxp.com/files/32bit/doc/errata/KINETIS_K_0N36M.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately the Reference Manual revisions take some time, so the change has not made it to the manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 18 Jun 2016 15:27:50 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2016-06-18T15:27:50Z</dc:date>
    <item>
      <title>MK02FN Flashloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02FN-Flashloader/m-p/547027#M33351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The MK02FN has a Flashloader but for I2C / UART the data sheet states PTC10,PTC11 / PTE0,PTE1 are used but these pins are not available on the 32 pin and 48 pin devices, can the Flashloader only be used with 64 pin devices ?&lt;/P&gt;&lt;P&gt;Furthermore PTC10,PTC11 are not routed to the I2C peripheral, is the I2C bit-banged in a 64 pin device ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help - is the above true or is there a data sheet error ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Ken Roberts&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Jun 2016 08:07:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02FN-Flashloader/m-p/547027#M33351</guid>
      <dc:creator>kenchill</dc:creator>
      <dc:date>2016-06-18T08:07:03Z</dc:date>
    </item>
    <item>
      <title>Re: MK02FN Flashloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02FN-Flashloader/m-p/547028#M33352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ken Roberts:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please read the response from colleague Carlos Chavez in the next thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/338502"&gt;FlashLoader on Kinetis MK02, Incorrect Peripherals, Error in Reference Manual&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The errata is already in place: &lt;A href="http://cache.nxp.com/files/32bit/doc/errata/KINETIS_K_0N36M.pdf" title="http://cache.nxp.com/files/32bit/doc/errata/KINETIS_K_0N36M.pdf"&gt;http://cache.nxp.com/files/32bit/doc/errata/KINETIS_K_0N36M.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately the Reference Manual revisions take some time, so the change has not made it to the manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Jun 2016 15:27:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02FN-Flashloader/m-p/547028#M33352</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-06-18T15:27:50Z</dc:date>
    </item>
  </channel>
</rss>