<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Deadtime insertion on FTM2 with FRDM-KE06Z</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Deadtime-insertion-on-FTM2-with-FRDM-KE06Z/m-p/542775#M33227</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Found the problem. Deadtime insertion doesn't work when fixed frequency clock is selected instead of system clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Jul 2016 12:54:49 GMT</pubDate>
    <dc:creator>brunotremblay</dc:creator>
    <dc:date>2016-07-07T12:54:49Z</dc:date>
    <item>
      <title>Deadtime insertion on FTM2 with FRDM-KE06Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Deadtime-insertion-on-FTM2-with-FRDM-KE06Z/m-p/542774#M33226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;I'm trying to the FTM2 channels 0 to 3 to generate Phase-shift PWM signal with the FRMD-KE06Z board as explained in the appnote "AN5142 Features of the FlexTimer Module" in the section 3.4. For generating Phase-shift signals there is no problem. It's easy to change the amount of phase-shift. However, I don't see any deadtime between the complementary channels CH0 and CH1 or CH2 and CH3. The only changes I made from AN5142 is using SIM_SCGC instead of SIM_SCGC6 to enable FTM2 module clock and changing FTM0_ for FTM2_.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to change the value in the FTM2_DEADTIME register, but at the scope screen's there's no deadtime.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the values of the registers:&lt;/P&gt;&lt;P&gt;SIM_SCGC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00003080&lt;/P&gt;&lt;P&gt;FTM2_SC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000010&lt;/P&gt;&lt;P&gt;FTM2_MOD&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x000003E8&lt;/P&gt;&lt;P&gt;FTM2_C0SC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000008&lt;/P&gt;&lt;P&gt;FTM2_C0V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x0000000A&lt;/P&gt;&lt;P&gt;FTM2_C1SC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000008&lt;/P&gt;&lt;P&gt;FTM2_C1V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x000001FE&lt;/P&gt;&lt;P&gt;FTM2_C2SC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000008&lt;/P&gt;&lt;P&gt;FTM2_C2V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x000000FA&lt;/P&gt;&lt;P&gt;FTM2_C3SC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000008&lt;/P&gt;&lt;P&gt;FTM2_C3V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x000002EE&lt;/P&gt;&lt;P&gt;FTM2_MODE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000005&lt;/P&gt;&lt;P&gt;FTM2_COMBINE&amp;nbsp; 0x00001313&lt;/P&gt;&lt;P&gt;FTM2_DEADTIME 0x0000001E&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2016 16:01:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Deadtime-insertion-on-FTM2-with-FRDM-KE06Z/m-p/542774#M33226</guid>
      <dc:creator>brunotremblay</dc:creator>
      <dc:date>2016-07-06T16:01:31Z</dc:date>
    </item>
    <item>
      <title>Re: Deadtime insertion on FTM2 with FRDM-KE06Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Deadtime-insertion-on-FTM2-with-FRDM-KE06Z/m-p/542775#M33227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Found the problem. Deadtime insertion doesn't work when fixed frequency clock is selected instead of system clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 12:54:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Deadtime-insertion-on-FTM2-with-FRDM-KE06Z/m-p/542775#M33227</guid>
      <dc:creator>brunotremblay</dc:creator>
      <dc:date>2016-07-07T12:54:49Z</dc:date>
    </item>
  </channel>
</rss>