<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Driver stepper motor ,KEA  or  KV?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-stepper-motor-KEA-or-KV/m-p/542209#M33200</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now there is a&amp;nbsp; medical automatic&amp;nbsp; injector instrument&amp;nbsp; project need&amp;nbsp; a MCU to control a stepper motor .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MC34932 is planed to be&amp;nbsp; as the driver .&lt;/P&gt;&lt;P&gt;The KVxx is dedicated for motor driver . But the KEA xx seems more reliable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KEA series&amp;nbsp;&amp;nbsp; and&amp;nbsp; KVxx&amp;nbsp; series&amp;nbsp; which is the best choice?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jul 2016 08:17:35 GMT</pubDate>
    <dc:creator>kigerzhang</dc:creator>
    <dc:date>2016-07-06T08:17:35Z</dc:date>
    <item>
      <title>Driver stepper motor ,KEA  or  KV?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-stepper-motor-KEA-or-KV/m-p/542209#M33200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now there is a&amp;nbsp; medical automatic&amp;nbsp; injector instrument&amp;nbsp; project need&amp;nbsp; a MCU to control a stepper motor .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MC34932 is planed to be&amp;nbsp; as the driver .&lt;/P&gt;&lt;P&gt;The KVxx is dedicated for motor driver . But the KEA xx seems more reliable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KEA series&amp;nbsp;&amp;nbsp; and&amp;nbsp; KVxx&amp;nbsp; series&amp;nbsp; which is the best choice?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2016 08:17:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-stepper-motor-KEA-or-KV/m-p/542209#M33200</guid>
      <dc:creator>kigerzhang</dc:creator>
      <dc:date>2016-07-06T08:17:35Z</dc:date>
    </item>
    <item>
      <title>Re: Driver stepper motor ,KEA  or  KV?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-stepper-motor-KEA-or-KV/m-p/542210#M33201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is really depend on your application, the requirement of your stepper motor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis V Series MCUs are based upon the ARM&lt;SUP&gt;®&lt;/SUP&gt; Cortex&lt;SUP&gt;®&lt;/SUP&gt;-M0+, Cortex-M4 and Cortex-M7 cores and are designed for a wide range of BLDC, PMSM and ACIM motor control and digital power conversion applications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Kinetis EA series is an entry point to the broad ARM ecosystem and features: &lt;/P&gt;&lt;UL&gt;&lt;LI&gt;A low-power ARM Cortex-M0+ core and 8–128 KB of embedded flash&lt;/LI&gt;&lt;LI&gt;Excellent EMC/ESD, high temperature and low radiated emissions&lt;/LI&gt;&lt;LI&gt;Scalable, highly robust performance solution for cost-sensitive automotive applications.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached you will find a PPT on this topic maybe helpful to you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2016 08:16:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Driver-stepper-motor-KEA-or-KV/m-p/542210#M33201</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-07-14T08:16:14Z</dc:date>
    </item>
  </channel>
</rss>