<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: LIN Bootloader</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-Bootloader/m-p/541171#M33141</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, any update to the bootloader that would work on S32k116 and support LIN?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Mar 2020 23:05:10 GMT</pubDate>
    <dc:creator>perig_vennetier</dc:creator>
    <dc:date>2020-03-13T23:05:10Z</dc:date>
    <item>
      <title>LIN Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-Bootloader/m-p/541169#M33139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I´m using a S32k14x (or plan to use) in a automotive application.&lt;/P&gt;&lt;P&gt;The only connection to the outside world in a LIN bus. So, a UART port together with a LIN transceiver should be fine.&lt;/P&gt;&lt;P&gt;However, my question concerns the ROM-based bootloader and if it possible to use the in a "LIN setup".&lt;/P&gt;&lt;P&gt;With that I mean that once the host has send the command to reboot and start in bootloader mode (using a LIN 2.0 Protocol), it could start sending commands by the protocol defined by the NXP bootloader implementation.&lt;/P&gt;&lt;P&gt;I´m not too familiar with the LIN interface but would it be possible to use the UART bootloader via a LIN transceiver? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 19:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-Bootloader/m-p/541169#M33139</guid>
      <dc:creator>jannebozz</dc:creator>
      <dc:date>2016-06-16T19:38:15Z</dc:date>
    </item>
    <item>
      <title>Re: LIN Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-Bootloader/m-p/541170#M33140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;S32K144 is supported by Rappid bootloader. Currently the bootloader supports UART and CAN. It can be downloaded here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=RAPPID_BOOTLOADER_UTILITY" title="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=RAPPID_BOOTLOADER_UTILITY"&gt;RAppID Boot Loader Utility&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LIN and UART are not compatible buses, so it is not possible to use the bootloader. The solution is either to use UART or CAN in your application, so Rappid bootloader can be used, or write own flash resident bootloader which will use LIN interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 06:00:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-Bootloader/m-p/541170#M33140</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2016-06-21T06:00:42Z</dc:date>
    </item>
    <item>
      <title>Re: LIN Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-Bootloader/m-p/541171#M33141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, any update to the bootloader that would work on S32k116 and support LIN?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 23:05:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-Bootloader/m-p/541171#M33141</guid>
      <dc:creator>perig_vennetier</dc:creator>
      <dc:date>2020-03-13T23:05:10Z</dc:date>
    </item>
    <item>
      <title>Re: LIN Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-Bootloader/m-p/541172#M33142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Perig,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;currently there are no plans to support LIN bootloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2020 05:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-Bootloader/m-p/541172#M33142</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2020-03-17T05:06:11Z</dc:date>
    </item>
    <item>
      <title>Re: LIN Bootloader</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-Bootloader/m-p/1781136#M65847</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi, any update to the bootloader that would works on S32k144 and support LIN communication to develop an LIN bootloader?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Dec 2023 07:28:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-Bootloader/m-p/1781136#M65847</guid>
      <dc:creator>Mithra</dc:creator>
      <dc:date>2023-12-29T07:28:00Z</dc:date>
    </item>
  </channel>
</rss>