<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KE06 KBI question</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KBI-question/m-p/540768#M33122</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, I just wanted to make sure it was a typo and not a limitation that only 8 of the 32 pins can be enabled at a time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jul 2016 12:15:08 GMT</pubDate>
    <dc:creator>davidsherman</dc:creator>
    <dc:date>2016-07-06T12:15:08Z</dc:date>
    <item>
      <title>KE06 KBI question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KBI-question/m-p/540765#M33119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking into the KE06 reference manual, I noticed something I hadn't before.&amp;nbsp; On page 698, it says "The KBI module allows up to eight pins to act as additional interrupt sources."&amp;nbsp; Does this mean only 8 pins can be enabled at a time?&amp;nbsp; That seems strange if there are 32 pins available to the KBI.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2016 16:57:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KBI-question/m-p/540765#M33119</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2016-07-05T16:57:59Z</dc:date>
    </item>
    <item>
      <title>Re: KE06 KBI question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KBI-question/m-p/540766#M33120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I haven't noticed any restrictions so it is probably a cut-and-paste error in the manual since the text is shared with the KE02, which has an 8 bit KBI controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2016 17:34:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KBI-question/m-p/540766#M33120</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-07-05T17:34:43Z</dc:date>
    </item>
    <item>
      <title>Re: KE06 KBI question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KBI-question/m-p/540767#M33121</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Just as Mark have said, it is the KE06 reference manual error, KE06 each KBI module have 32 pin, so the KBI module allows up to 32 pins to act as additional interrupts sources.&lt;/P&gt;&lt;P&gt;&amp;nbsp; From the interrupt vector assignments, we also can find it.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="54.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/36649i025863065D82F6B1/image-size/large?v=v2&amp;amp;px=999" role="button" title="54.jpg" alt="54.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact me!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2016 06:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KBI-question/m-p/540767#M33121</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-07-06T06:54:29Z</dc:date>
    </item>
    <item>
      <title>Re: KE06 KBI question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KBI-question/m-p/540768#M33122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, I just wanted to make sure it was a typo and not a limitation that only 8 of the 32 pins can be enabled at a time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2016 12:15:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KE06-KBI-question/m-p/540768#M33122</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2016-07-06T12:15:08Z</dc:date>
    </item>
  </channel>
</rss>