<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Default_Handler happens</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-Handler-happens/m-p/539825#M33079</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The only thing that comes to mind is if PTB4 is also being configured as an output.&amp;nbsp; That is the NMI pin, which is enabled by default.&amp;nbsp; Are you configuring all of the port B pins, or only PTB5?&amp;nbsp; Could something else be pulling PTB4 low?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 15:54:55 GMT</pubDate>
    <dc:creator>davidsherman</dc:creator>
    <dc:date>2016-06-16T15:54:55Z</dc:date>
    <item>
      <title>Default_Handler happens</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-Handler-happens/m-p/539824#M33078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using KEAZ128M microcontroller. I meet a problem. When I config PTB5 as GPIO output, the Default_Handler() below will be triggered.I am using Code Warrior. And I don't use Processor Expert.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am really confused..what is the reason.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Haizhou&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 09:38:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-Handler-happens/m-p/539824#M33078</guid>
      <dc:creator>haizhougeng</dc:creator>
      <dc:date>2016-06-16T09:38:07Z</dc:date>
    </item>
    <item>
      <title>Re: Default_Handler happens</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-Handler-happens/m-p/539825#M33079</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The only thing that comes to mind is if PTB4 is also being configured as an output.&amp;nbsp; That is the NMI pin, which is enabled by default.&amp;nbsp; Are you configuring all of the port B pins, or only PTB5?&amp;nbsp; Could something else be pulling PTB4 low?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 15:54:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-Handler-happens/m-p/539825#M33079</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2016-06-16T15:54:55Z</dc:date>
    </item>
    <item>
      <title>Re: Default_Handler happens</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-Handler-happens/m-p/539826#M33080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks David.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set NMIE bit 0 on SIM_SOPT0 register. And Default Handler don't happens.&lt;/P&gt;&lt;P&gt;But I am still confused why PTB5 will trigger it. Maybe I should check my PCB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 02:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-Handler-happens/m-p/539826#M33080</guid>
      <dc:creator>haizhougeng</dc:creator>
      <dc:date>2016-06-17T02:13:14Z</dc:date>
    </item>
    <item>
      <title>Re: Default_Handler happens</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-Handler-happens/m-p/539827#M33081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Haizhou,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As David mentions maybe the problem is on the code that configures the PTB5 pin as an output, could you share your project to see if I can reproduce the issue on my side?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos Mendoza&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jun 2016 17:44:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Default-Handler-happens/m-p/539827#M33081</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2016-06-20T17:44:04Z</dc:date>
    </item>
  </channel>
</rss>