<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: GPIO protection</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-protection/m-p/539104#M33070</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Only using a series 10K resistor for EOS protection is not permitted.&lt;BR /&gt;For Digital inputs only have a diode to VSS, allowing negative injection but not positive injection&lt;BR /&gt;Please check below picture about K10 GPIO pin protection circuit:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2883i3DD892F18C0309D0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Dig Pad for digital function pin, such GPIO pin; Ana Pad for analog function pin, such as ADC channel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other recommend way is using a TVS diode between 10K serial resistor with K10 GPIO pin.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Aug 2016 04:46:05 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2016-08-26T04:46:05Z</dc:date>
    <item>
      <title>GPIO protection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-protection/m-p/539101#M33067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to datasheet K10P144M100SF2V2 GPIO &lt;SPAN style="color: #e23d39;"&gt;only have clamp diode to VSS&lt;/SPAN&gt;. I need EOS protection up to +24V. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 25.95px;"&gt;I can experiment and find what works but I will like to understand GPIO characteristics.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I use a series 10K resistor for protection?&lt;/P&gt;&lt;P&gt;Will it cause latchup because 24V &amp;gt; Max 5~5.5V even though it can't drive latch up current of 100ma?&lt;/P&gt;&lt;P&gt;What will be the voltage at pin?&lt;/P&gt;&lt;P&gt;What is the reverse break down voltage of clamp diode?&lt;/P&gt;&lt;P&gt;Will I I definitely need another clamp diode to VDD as well ? Why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Aug 2016 08:27:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-protection/m-p/539101#M33067</guid>
      <dc:creator>tejpalsingh</dc:creator>
      <dc:date>2016-08-18T08:27:42Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO protection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-protection/m-p/539102#M33068</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K10 100MHz product all GPIO pins have 5 V tolerance.&lt;/P&gt;&lt;P&gt;All 5 V tolerant digital I/O pins are internally clamped to VSS through an ESD protection diode. There is no diode connection to VDD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Circuit design and PCB layout are fundamental in preventing EOS conditions from reaching the device.&lt;/P&gt;&lt;P&gt;There are several publications that offer great advice on properly designing circuits to prevent overstress conditions.&lt;/P&gt;&lt;P&gt;The recommendations in the publications concentrate on the following:&lt;/P&gt;&lt;P&gt;• Clean VCC and VSS Supplies:&lt;/P&gt;&lt;P&gt;- Avoid excessive ringing and power-up overshoot/undershoot&lt;/P&gt;&lt;P&gt;• Controlled VCC Ramp at Power-up and Power-Down:&lt;/P&gt;&lt;P&gt;- Too fast power-up or power-down could cause excessive inrush currents through the circuit&lt;/P&gt;&lt;P&gt;• Proper Power/Ground:&lt;/P&gt;&lt;P&gt;- Avoid ground loops and ground differentials&lt;/P&gt;&lt;P&gt;• Correct Decoupling Capacitor Values:&lt;/P&gt;&lt;P&gt;- Essential for filtering high-frequency spikes&lt;/P&gt;&lt;P&gt;• Data Bus Contentions&lt;/P&gt;&lt;P&gt;• Connecting External Cable to an Unprotected I/O Port&lt;/P&gt;&lt;P&gt;• Proper Component Placement&lt;/P&gt;&lt;P&gt;• Short Trace Lengths&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K10 most GPIO pin are in high impedance status during power up.&lt;/P&gt;&lt;P&gt;Using a current-limiting resistor and a ferrite bead with a capacitor to ground will limit the energy transferred to a pin during an EOS event.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Aug 2016 08:19:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-protection/m-p/539102#M33068</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-08-23T08:19:56Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO protection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-protection/m-p/539103#M33069</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Ma Hui,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I will like to thank you for replying and also thanks for a polite and long reply with known generic information.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;BTW I have read some of your replies here and I have experience in interacting with many semi vendor support sites. So I am aware what kind I support I expect.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I don't know what is your official association with NXP and if this reply is on behalf of NXP.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;If this is official response from NXP support staff then it is pathetic and useless generic response.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;If you are replying as a community gesture. I have a suggestion for you. Please only reply if you have specific answers.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;But NXP is not exception response at most vendor community sites is poor and sometimes I have to get answers by approaching official customer support.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Tejpal&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 00:06:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-protection/m-p/539103#M33069</guid>
      <dc:creator>tejpalsingh</dc:creator>
      <dc:date>2016-08-24T00:06:25Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO protection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-protection/m-p/539104#M33070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Only using a series 10K resistor for EOS protection is not permitted.&lt;BR /&gt;For Digital inputs only have a diode to VSS, allowing negative injection but not positive injection&lt;BR /&gt;Please check below picture about K10 GPIO pin protection circuit:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2883i3DD892F18C0309D0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Dig Pad for digital function pin, such GPIO pin; Ana Pad for analog function pin, such as ADC channel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other recommend way is using a TVS diode between 10K serial resistor with K10 GPIO pin.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Aug 2016 04:46:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-protection/m-p/539104#M33070</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-08-26T04:46:05Z</dc:date>
    </item>
  </channel>
</rss>