<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: How to use TWR-K60F120M &amp; TWR-SER?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-TWR-K60F120M-TWR-SER/m-p/208018#M3293</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mellisa,&lt;/P&gt;&lt;P&gt; Is this the same case for TWR-K20D72M and TWR-SER? I'm getting signals on the Tx pin of the K20 but not from the final Db9 connector..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;H.S.Srinivas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Oct 2014 02:21:29 GMT</pubDate>
    <dc:creator>srinivashimakun</dc:creator>
    <dc:date>2014-10-17T02:21:29Z</dc:date>
    <item>
      <title>How to use TWR-K60F120M &amp; TWR-SER?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-TWR-K60F120M-TWR-SER/m-p/208015#M3290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;currently I'm trying to use the mentioned tower modules. In the schematic files of both modules I have seen that the TWR-SER module uses the elevator pins A43/44 as RX/TX source. The CPU module maps UART5 to this pins. But this interface is also used for the OSBDM stuff. So is it right that the TWR-SER module isn't usable with the TWR-K60F120M?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;flo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Oct 2012 07:21:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-TWR-K60F120M-TWR-SER/m-p/208015#M3290</guid>
      <dc:creator>mich1985</dc:creator>
      <dc:date>2012-10-04T07:21:35Z</dc:date>
    </item>
    <item>
      <title>Re: How to use TWR-K60F120M &amp; TWR-SER?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-TWR-K60F120M-TWR-SER/m-p/208016#M3291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The OS-BDM circuit includes a serial terminal function. You can communicate with the board using a terminal using the P&amp;amp;E terminal utility connected to the OS-BDM -or- you can use your favorite terminal emulator application connected to the OS-BDM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The OS-BDM circuit will not interfere with use of the TWR-SER as long as you don't try to use the P&amp;amp;E terminal utility at the same time that you are using the UART port through the TWR-SER. Just pick the one you want to use, and make sure you only use one at a time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Melissa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2012 18:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-TWR-K60F120M-TWR-SER/m-p/208016#M3291</guid>
      <dc:creator>melissa_hunter</dc:creator>
      <dc:date>2012-10-23T18:44:09Z</dc:date>
    </item>
    <item>
      <title>Re: How to use TWR-K60F120M &amp; TWR-SER?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-TWR-K60F120M-TWR-SER/m-p/208017#M3292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello and thx for your reply. Because I wasn't sure if OSBDM really wouldn't interfere with the TWR-SER serial interface so I have removed R63 (UART5_TX) &amp;amp; R65 (UART5_RX) on TWR-K60F120M for my evaluation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;flo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2012 19:32:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-TWR-K60F120M-TWR-SER/m-p/208017#M3292</guid>
      <dc:creator>mich1985</dc:creator>
      <dc:date>2012-10-24T19:32:25Z</dc:date>
    </item>
    <item>
      <title>Re: How to use TWR-K60F120M &amp; TWR-SER?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-TWR-K60F120M-TWR-SER/m-p/208018#M3293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mellisa,&lt;/P&gt;&lt;P&gt; Is this the same case for TWR-K20D72M and TWR-SER? I'm getting signals on the Tx pin of the K20 but not from the final Db9 connector..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;H.S.Srinivas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Oct 2014 02:21:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-TWR-K60F120M-TWR-SER/m-p/208018#M3293</guid>
      <dc:creator>srinivashimakun</dc:creator>
      <dc:date>2014-10-17T02:21:29Z</dc:date>
    </item>
    <item>
      <title>Re: How to use TWR-K60F120M &amp; TWR-SER?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-TWR-K60F120M-TWR-SER/m-p/208019#M3294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Srinivas Himakuntala:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it is the same situation. In this case for TWR-20D72M&amp;nbsp; the pins PTE0/PTE1 for UART1 are shared between OSBDM virtual port and TWR-SER. As Melissa mentioned, there should be no problem as long as you only use one interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you do not see the signal in DB9, check the jumpers J17 and J19. Both should be in position &lt;STRONG&gt;1-2&lt;/STRONG&gt;. Also make sure that TWR-SER has power.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46841i05FDDD4F1F75C884/image-size/large?v=v2&amp;amp;px=999" title="TWR_SER.png" alt="TWR_SER.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Oct 2014 04:23:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-TWR-K60F120M-TWR-SER/m-p/208019#M3294</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-10-17T04:23:58Z</dc:date>
    </item>
  </channel>
</rss>