<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Why Does the Kinetis K26 micro flash fail in 2 specific sectors consistently. in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Does-the-Kinetis-K26-micro-flash-fail-in-2-specific-sectors/m-p/531836#M32839</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The issue appears to be related to the K65f180m "flash_demo" project for IAR IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've run the demo reconfigured for a K26 on our board.&lt;/P&gt;&lt;P&gt;In the demo, we erase a part of the upper pflash block (/w verification) ( 0xFE000 - 0x100000).&lt;/P&gt;&lt;P&gt;Later in the demo, we swap the flash blocks (0,1 -&amp;gt; 2,3).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our application, erasing any of the first sixteen bytes of the 0xFE000 sector while the SWAP bit of FTFE_FCNFG register is SET causes the FPVIOL flag of the FTFE_FSTAT register to trigger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not going to put any more time into this as it does not effect our application when we do not run the demo application.&lt;/P&gt;&lt;P&gt;We also do not use the flash swap feature.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Jul 2016 19:30:54 GMT</pubDate>
    <dc:creator>ericdurst</dc:creator>
    <dc:date>2016-07-18T19:30:54Z</dc:date>
    <item>
      <title>Why Does the Kinetis K26 micro flash fail in 2 specific sectors consistently.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Does-the-Kinetis-K26-micro-flash-fail-in-2-specific-sectors/m-p/531835#M32838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've now had 2 micros fail in the exact same flash sector without approaching the erase cycle limit. To be fair, I haven't kept track of how many erase cycles I've done, but It would definitely be between 100 to 200 flash erase cycles.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The flash sectors that fail are located at 0xFE000 and 0x1FE000.&lt;/P&gt;&lt;P&gt;I get a FPVIOL error when I try to erase these sectors.&lt;/P&gt;&lt;P&gt;It appears only the first 16 bytes are failing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What might cause this? Is there a known mask issue? did I get unlucky twice?&lt;/P&gt;&lt;P&gt;Let me know if more information is required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2016 16:49:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Does-the-Kinetis-K26-micro-flash-fail-in-2-specific-sectors/m-p/531835#M32838</guid>
      <dc:creator>ericdurst</dc:creator>
      <dc:date>2016-07-01T16:49:16Z</dc:date>
    </item>
    <item>
      <title>Re: Why Does the Kinetis K26 micro flash fail in 2 specific sectors consistently.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Does-the-Kinetis-K26-micro-flash-fail-in-2-specific-sectors/m-p/531836#M32839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The issue appears to be related to the K65f180m "flash_demo" project for IAR IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've run the demo reconfigured for a K26 on our board.&lt;/P&gt;&lt;P&gt;In the demo, we erase a part of the upper pflash block (/w verification) ( 0xFE000 - 0x100000).&lt;/P&gt;&lt;P&gt;Later in the demo, we swap the flash blocks (0,1 -&amp;gt; 2,3).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our application, erasing any of the first sixteen bytes of the 0xFE000 sector while the SWAP bit of FTFE_FCNFG register is SET causes the FPVIOL flag of the FTFE_FSTAT register to trigger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not going to put any more time into this as it does not effect our application when we do not run the demo application.&lt;/P&gt;&lt;P&gt;We also do not use the flash swap feature.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jul 2016 19:30:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Does-the-Kinetis-K26-micro-flash-fail-in-2-specific-sectors/m-p/531836#M32839</guid>
      <dc:creator>ericdurst</dc:creator>
      <dc:date>2016-07-18T19:30:54Z</dc:date>
    </item>
    <item>
      <title>Re: Why Does the Kinetis K26 micro flash fail in 2 specific sectors consistently.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Does-the-Kinetis-K26-micro-flash-fail-in-2-specific-sectors/m-p/531837#M32840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;Thanks for your sharing,&lt;/P&gt;&lt;P&gt;And I was wondering if you can tell me the exactly chip number of K26 you use.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 08:58:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Does-the-Kinetis-K26-micro-flash-fail-in-2-specific-sectors/m-p/531837#M32840</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-07-19T08:58:35Z</dc:date>
    </item>
    <item>
      <title>Re: Why Does the Kinetis K26 micro flash fail in 2 specific sectors consistently.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Does-the-Kinetis-K26-micro-flash-fail-in-2-specific-sectors/m-p/531838#M32841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Turning on the 'swap' function TAKES OVER the indicated phrase in such block in EACH HALF of memory space.&amp;nbsp; You are NO LONGER 'free' to erase/write any part of those phrases.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 18:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Why-Does-the-Kinetis-K26-micro-flash-fail-in-2-specific-sectors/m-p/531838#M32841</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-07-19T18:03:04Z</dc:date>
    </item>
  </channel>
</rss>