<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollersのトピックfreedom board as programmer</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/freedom-board-as-programmer/m-p/530294#M32832</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a Freedom KE02 board I am using as a programmer for a stand-alone KE02 system.&amp;nbsp; I am using J7 as the programming interface, after disconnecting the dataline from the on-board KE02.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have to use the stand-alone system at 5V.&amp;nbsp; In order to keep using the Freedom board while powered up at 5V, I will disconnect V3.3 from J7.&amp;nbsp; Should I put a 1KOhm resistor in line with the SWD_DIO or CLK lines?&amp;nbsp; I am using TXD and RXD with 1KOhm resistors in line with those signals. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help, I also use FreeMaster so having the stand-alone and the Freedom boards connected while operating is required.&amp;nbsp; I just don't want to hurt anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Jul 2016 11:43:03 GMT</pubDate>
    <dc:creator>andyvoss</dc:creator>
    <dc:date>2016-07-22T11:43:03Z</dc:date>
    <item>
      <title>freedom board as programmer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/freedom-board-as-programmer/m-p/530294#M32832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a Freedom KE02 board I am using as a programmer for a stand-alone KE02 system.&amp;nbsp; I am using J7 as the programming interface, after disconnecting the dataline from the on-board KE02.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have to use the stand-alone system at 5V.&amp;nbsp; In order to keep using the Freedom board while powered up at 5V, I will disconnect V3.3 from J7.&amp;nbsp; Should I put a 1KOhm resistor in line with the SWD_DIO or CLK lines?&amp;nbsp; I am using TXD and RXD with 1KOhm resistors in line with those signals. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help, I also use FreeMaster so having the stand-alone and the Freedom boards connected while operating is required.&amp;nbsp; I just don't want to hurt anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jul 2016 11:43:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/freedom-board-as-programmer/m-p/530294#M32832</guid>
      <dc:creator>andyvoss</dc:creator>
      <dc:date>2016-07-22T11:43:03Z</dc:date>
    </item>
    <item>
      <title>Re: freedom board as programmer</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/freedom-board-as-programmer/m-p/530295#M32833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andy,&lt;/P&gt;&lt;P&gt;Regarding to your query, I'd highly recommend you to use the 3.3-5 logic convert chip. I think it's good way to work it out.&lt;/P&gt;&lt;P&gt;You can learn the more information about it by through the link as below.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/documents/application_note/AN240.pdf" title="http://www.nxp.com/documents/application_note/AN240.pdf"&gt;http://www.nxp.com/documents/application_note/AN240.pdf&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 04:38:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/freedom-board-as-programmer/m-p/530295#M32833</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-07-25T04:38:39Z</dc:date>
    </item>
  </channel>
</rss>