<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PWM value update with PE Init_FTM component in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526768#M32768</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks to you, the value update is now working. &lt;/P&gt;&lt;P&gt;By HAL, I think you mean the LDD components? Initialy, I was wanting to use the Init_FTM componement because in it I was able to initialize all 4 channels with combine, complementary and deadtime at the same time. By using the LDD, I must have a component by channel and do the rest of the settings in my code. At the end, it's longuer but it finaly works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bruno &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Aug 2016 13:22:02 GMT</pubDate>
    <dc:creator>brunotremblay</dc:creator>
    <dc:date>2016-08-17T13:22:02Z</dc:date>
    <item>
      <title>PWM value update with PE Init_FTM component</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526764#M32764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to generate a phase shift PWM signal using 4 channel for the FTM2 on a MKE06Z. I have no problem initialize the PE Init_FTM to generate the signals I want, but I can't change the values (FTM_CnV) register at runtime with the following interface : &lt;SPAN style="font-family: 'courier new', courier;"&gt;FTM_PDD_WriteChannelValueReg(FTM2_BASE_PTR,FTM_PDD_CHANNEL_2,Shift);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've try to call it periodicaly or put it in the OverflowInterrupt, but the value in the register won't change. In the reference manual, it's not clearly explain when, where or how to change or update the channel value. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried the solution of the &lt;A href="https://community.nxp.com/message/804458"&gt;Update PWM period on runtime&lt;/A&gt; post, it works ok for one channel, but I can't combine two channels. Do someone have an idea?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2016 18:45:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526764#M32764</guid>
      <dc:creator>brunotremblay</dc:creator>
      <dc:date>2016-08-15T18:45:09Z</dc:date>
    </item>
    <item>
      <title>Re: PWM value update with PE Init_FTM component</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526765#M32765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Hi Bruno,&lt;/P&gt;&lt;P&gt;CnV is double buffered register as is Modulo and some other. So when you writing value to it you are actually writing value to its buffer. To update register with its buffer value you need to make trigger cmd(hardware or software). The easiest way is to use software trigger. Using HAL it is :&lt;/P&gt;&lt;P&gt;FTM_HAL_SetSoftwareTriggerCmd(FTM2,true);&lt;/P&gt;&lt;P&gt;be sure to set software trigger while initializating FTM.&lt;/P&gt;&lt;P&gt; Hope it will help,&lt;/P&gt;&lt;P&gt;Alexey.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2016 20:59:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526765#M32765</guid>
      <dc:creator>alexeyusoltsev</dc:creator>
      <dc:date>2016-08-15T20:59:09Z</dc:date>
    </item>
    <item>
      <title>Re: PWM value update with PE Init_FTM component</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526766#M32766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexey,&lt;/P&gt;&lt;P&gt;Thanks for your reply. Since I use the Init_FTM component, the only macros available are listed below. I don't have any general software trigger command. I tried with initializing all the software trigger with each trigger macro but the value still won't update. Can you tell me which bit in which register the "&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; font-size: 14px;"&gt;FTM_HAL_SetSoftwareTriggerCmd(FTM2,true)" &lt;/SPAN&gt;macro take action?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Software trigger macros available:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Component initialization :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3630iF4004FC54289181C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3684i9DA2F6AB506EDD29/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I found the "AN4560 PWM Synchronisation Using Kinetis Flextimers" app. note, maybe with that I will find something to help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 13:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526766#M32766</guid>
      <dc:creator>brunotremblay</dc:creator>
      <dc:date>2016-08-16T13:20:06Z</dc:date>
    </item>
    <item>
      <title>Re: PWM value update with PE Init_FTM component</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526767#M32767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Hi again!&lt;/P&gt;&lt;P&gt;Yes, this is very helpfull appnote.&lt;/P&gt;&lt;P&gt;Init component:&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3978i78853BBD48C220B6/image-size/large?v=v2&amp;amp;px=999" title="INIT.jpg" alt="INIT.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and to send software trigger you need to FTM2_SYNC|=FTM_SYNC_SWSYNC(1);&lt;/P&gt;&lt;P&gt;If it will not work check in the debugger mode SYNCCONF register in the FTM.&lt;/P&gt;&lt;P&gt; Why don't you want to use HAL instead of INIT component?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 13:51:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526767#M32767</guid>
      <dc:creator>alexeyusoltsev</dc:creator>
      <dc:date>2016-08-16T13:51:45Z</dc:date>
    </item>
    <item>
      <title>Re: PWM value update with PE Init_FTM component</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526768#M32768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks to you, the value update is now working. &lt;/P&gt;&lt;P&gt;By HAL, I think you mean the LDD components? Initialy, I was wanting to use the Init_FTM componement because in it I was able to initialize all 4 channels with combine, complementary and deadtime at the same time. By using the LDD, I must have a component by channel and do the rest of the settings in my code. At the end, it's longuer but it finaly works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bruno &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Aug 2016 13:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526768#M32768</guid>
      <dc:creator>brunotremblay</dc:creator>
      <dc:date>2016-08-17T13:22:02Z</dc:date>
    </item>
    <item>
      <title>Re: PWM value update with PE Init_FTM component</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526769#M32769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Bruno,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I also used PDD. &amp;nbsp;Which command use for "&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;value update". Please tell me. Many thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp; :smileyhappy:&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Nov 2016 04:08:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526769#M32769</guid>
      <dc:creator>tommyliu</dc:creator>
      <dc:date>2016-11-22T04:08:11Z</dc:date>
    </item>
    <item>
      <title>Re: PWM value update with PE Init_FTM component</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526770#M32770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tommy,&lt;/P&gt;&lt;P&gt;If software trigger is initialized, FTM_PDD_PWMSoftwareTrigger() can be used to trigger "&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;value update&lt;/SPAN&gt;".&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5820i1818A4D8E3DA8B60/image-size/large?v=v2&amp;amp;px=999" title="FTM_PDD_PWMSoftwareTrigger.png" alt="FTM_PDD_PWMSoftwareTrigger.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the chapter "26.4.11.6 C(n)V and C(n+1)V register synchronization" in&amp;nbsp;&lt;A href="http://www.nxp.com/assets/documents/data/en/reference-manuals/MKE06P80M48SF0RM.pdf"&gt;MKE06P80M48SF0RM&lt;/A&gt; we can know that: The synchronization mechanism is the same as the MOD register synchronization.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5907i4E2E6C897D323F85/image-size/large?v=v2&amp;amp;px=999" title="26.4.11.6 C(n)V and C(n+1)V register synchronization.png" alt="26.4.11.6 C(n)V and C(n+1)V register synchronization.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So see chapter "26.4.11.4 MOD register synchronization":&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6000i36900F5E1D8E7797/image-size/large?v=v2&amp;amp;px=999" title="Figure 26-44. MOD register synchronization flowchart.png" alt="Figure 26-44. MOD register synchronization flowchart.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2017 08:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PWM-value-update-with-PE-Init-FTM-component/m-p/526770#M32770</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-01-04T08:20:11Z</dc:date>
    </item>
  </channel>
</rss>