<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is NXP Touch Software compatible with the Kenetis SDK 2.0 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-NXP-Touch-Software-compatible-with-the-Kenetis-SDK-2-0/m-p/520240#M32722</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am about to start a project with 3 cap touch buttons. Each button has it's own trace. I really have 2 questions. Do I need to use the NXP touch software to implement simple buttons? It seems to be geared more towards sliders and number pads.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The second question is whether or not that library is compatible with the newer SDK 2.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:41:57 GMT</pubDate>
    <dc:creator>davidfindlay</dc:creator>
    <dc:date>2016-06-15T17:41:57Z</dc:date>
    <item>
      <title>Is NXP Touch Software compatible with the Kenetis SDK 2.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-NXP-Touch-Software-compatible-with-the-Kenetis-SDK-2-0/m-p/520240#M32722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am about to start a project with 3 cap touch buttons. Each button has it's own trace. I really have 2 questions. Do I need to use the NXP touch software to implement simple buttons? It seems to be geared more towards sliders and number pads.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The second question is whether or not that library is compatible with the newer SDK 2.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:41:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-NXP-Touch-Software-compatible-with-the-Kenetis-SDK-2-0/m-p/520240#M32722</guid>
      <dc:creator>davidfindlay</dc:creator>
      <dc:date>2016-06-15T17:41:57Z</dc:date>
    </item>
    <item>
      <title>Re: Is NXP Touch Software compatible with the Kenetis SDK 2.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-NXP-Touch-Software-compatible-with-the-Kenetis-SDK-2-0/m-p/520241#M32723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;Yes, it is supported by the SDK 2.0.&amp;nbsp; Here is a useful start guide on this regard:&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-329432" title="https://community.nxp.com/docs/DOC-329432"&gt;https://community.nxp.com/docs/DOC-329432&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 07:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-NXP-Touch-Software-compatible-with-the-Kenetis-SDK-2-0/m-p/520241#M32723</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-06-17T07:24:25Z</dc:date>
    </item>
    <item>
      <title>Re: Is NXP Touch Software compatible with the Kenetis SDK 2.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-NXP-Touch-Software-compatible-with-the-Kenetis-SDK-2-0/m-p/520242#M32724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes but this guide clearly seems to imply you need the KSDK 1.2. And after attempting to run the installer it seems to be insisting on it. I get the following error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"The selected KSDK folder doesn't content Freescale KSDK 1.2"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 16:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-NXP-Touch-Software-compatible-with-the-Kenetis-SDK-2-0/m-p/520242#M32724</guid>
      <dc:creator>davidfindlay</dc:creator>
      <dc:date>2016-06-17T16:21:14Z</dc:date>
    </item>
    <item>
      <title>Re: Is NXP Touch Software compatible with the Kenetis SDK 2.0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-NXP-Touch-Software-compatible-with-the-Kenetis-SDK-2-0/m-p/520243#M32725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please see the following screenshot. The touch software seems to insist on SDK V 1.2 which I can not even figure out how to obtain anymore. I can only get 2.0 and 1.3. Both of these don't work when I attempt to install the library.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2752iF32B293085E52927/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2016 20:13:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-NXP-Touch-Software-compatible-with-the-Kenetis-SDK-2-0/m-p/520243#M32725</guid>
      <dc:creator>davidfindlay</dc:creator>
      <dc:date>2016-08-31T20:13:27Z</dc:date>
    </item>
  </channel>
</rss>