<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KL03 What is the minimum VDD for the VRef-regulator? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-What-is-the-minimum-VDD-for-the-VRef-regulator/m-p/519582#M32702</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;the Datasheets states an operating voltage-range for VDD and VDDA of 1.71...3.6V. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;The voltage-reference-module is equipped with a 1.75V regulator. It is also stated, that the regulator should be used&amp;nbsp; to get the full performance. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;I would like to opperate the device at low VCC, about 1.8V. Since the use of the chopper adds a 35ms delay (see topic &lt;/SPAN&gt;&lt;SPAN style="font-size: 12pt;"&gt;"KL03 Voltage Reference Start-up Time") to get the refernce running, I would like to use the regulator w/o the chopper. I assume, that this implies the need for a little higher VDDA as there must be some headroom for the regulator.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Q: What is the minimum VDDA for the use of the regulator for VREF w/o enabling the chopper?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Thanks in advance&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Gernot&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jun 2016 14:27:06 GMT</pubDate>
    <dc:creator>gernotmiksch</dc:creator>
    <dc:date>2016-06-13T14:27:06Z</dc:date>
    <item>
      <title>KL03 What is the minimum VDD for the VRef-regulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-What-is-the-minimum-VDD-for-the-VRef-regulator/m-p/519582#M32702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;the Datasheets states an operating voltage-range for VDD and VDDA of 1.71...3.6V. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;The voltage-reference-module is equipped with a 1.75V regulator. It is also stated, that the regulator should be used&amp;nbsp; to get the full performance. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;I would like to opperate the device at low VCC, about 1.8V. Since the use of the chopper adds a 35ms delay (see topic &lt;/SPAN&gt;&lt;SPAN style="font-size: 12pt;"&gt;"KL03 Voltage Reference Start-up Time") to get the refernce running, I would like to use the regulator w/o the chopper. I assume, that this implies the need for a little higher VDDA as there must be some headroom for the regulator.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Q: What is the minimum VDDA for the use of the regulator for VREF w/o enabling the chopper?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Thanks in advance&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;Gernot&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jun 2016 14:27:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-What-is-the-minimum-VDD-for-the-VRef-regulator/m-p/519582#M32702</guid>
      <dc:creator>gernotmiksch</dc:creator>
      <dc:date>2016-06-13T14:27:06Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 What is the minimum VDD for the VRef-regulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-What-is-the-minimum-VDD-for-the-VRef-regulator/m-p/519583#M32703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;First please be sure to make the VREFH &amp;lt; VDDA&amp;nbsp; in any case even in the low power mode. And with the marge that the difference between VREFH and VDDA can be max 100mV. If the difference VREFH - VDDA &amp;gt; 100mV the current starts to flow through the clamping diode to VDDA line that will made the chip damaged.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Fang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jun 2016 09:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-What-is-the-minimum-VDD-for-the-VRef-regulator/m-p/519583#M32703</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-06-14T09:04:48Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 What is the minimum VDD for the VRef-regulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-What-is-the-minimum-VDD-for-the-VRef-regulator/m-p/519584#M32704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Probably, I asked wrong.&lt;/P&gt;&lt;P&gt;I know, that VREFH should not exceed VDDA. My question is about the internal regulator of the VREF-module. This module delivers a reference of 1.2V nominal, using a bandgap-reference to ADC and CMP. The bandgab could be supplied by an internal regulator, which supplies 1.75V to the bandgap and is intended to suppress changes on VDD/VDDA. This regulator is enabled by setting VREF_SC[REGEN]. &lt;/P&gt;&lt;P&gt;The question was, what minimum VDDA is neccessary to keep the regulator in regulation. For example, if VDDA is between 1.71V and 1.75V, I assume, the regulator is out of regulation (if no chopper increases the VDDA before fed to the regulator).&lt;/P&gt;&lt;P&gt;Since the use of the chopper adds an enourmous ammount of time before the reference could be used, I want to avoid the chopper. But, to get advantages from a stabilized voltage fed to the reference, I would like to enable the regulator.&lt;/P&gt;&lt;P&gt;Since even low-drop-regulators need some headroom to regulate, I would like to know, how much it is.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Gernot&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jun 2016 11:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-What-is-the-minimum-VDD-for-the-VRef-regulator/m-p/519584#M32704</guid>
      <dc:creator>gernotmiksch</dc:creator>
      <dc:date>2016-06-14T11:24:32Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 What is the minimum VDD for the VRef-regulator?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-What-is-the-minimum-VDD-for-the-VRef-regulator/m-p/519585#M32705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, from what I understood, VREF is a module that has to be enable, hence, it is not always enable as you know.&amp;nbsp; And&amp;nbsp; VREF is not related with VREFH nor VREFL pins, so it is no relative with VDDA.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2016 08:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-What-is-the-minimum-VDD-for-the-VRef-regulator/m-p/519585#M32705</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-08-02T08:56:10Z</dc:date>
    </item>
  </channel>
</rss>