<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to power USB OTG in FRDM-K64F in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-power-USB-OTG-in-FRDM-K64F/m-p/516854#M32627</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to see if I can avoid soldering the FRDM-K64 board for this and I&amp;nbsp; need some further clarification from the documentation about the FRDM-K64F board. Without using the OpenSDA port, if my program uses the USB OTG port to interact with a device, is it enough to provide 5V through P5V_USB (Pin 10 of header J3) to power the board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Xavier&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Jun 2016 12:14:40 GMT</pubDate>
    <dc:creator>xavierx</dc:creator>
    <dc:date>2016-06-08T12:14:40Z</dc:date>
    <item>
      <title>How to power USB OTG in FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-power-USB-OTG-in-FRDM-K64F/m-p/516854#M32627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to see if I can avoid soldering the FRDM-K64 board for this and I&amp;nbsp; need some further clarification from the documentation about the FRDM-K64F board. Without using the OpenSDA port, if my program uses the USB OTG port to interact with a device, is it enough to provide 5V through P5V_USB (Pin 10 of header J3) to power the board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Xavier&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jun 2016 12:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-power-USB-OTG-in-FRDM-K64F/m-p/516854#M32627</guid>
      <dc:creator>xavierx</dc:creator>
      <dc:date>2016-06-08T12:14:40Z</dc:date>
    </item>
    <item>
      <title>Re: How to power USB OTG in FRDM-K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-power-USB-OTG-in-FRDM-K64F/m-p/516855#M32628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xavier,&lt;/P&gt;&lt;P&gt;Yes, I think so.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Jun 2016 02:57:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-power-USB-OTG-in-FRDM-K64F/m-p/516855#M32628</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-06-12T02:57:07Z</dc:date>
    </item>
  </channel>
</rss>