<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can bus clock in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-bus-clock/m-p/515874#M32622</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no 'inherent' rate for CPU or Bus clock, there are just 'maximums'.&amp;nbsp; Your general MCG clock setup will determine those.&amp;nbsp; I recommend running the CAN bit-rate-divisor functions directly from the input (XTAL) clock.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Jun 2016 11:27:02 GMT</pubDate>
    <dc:creator>egoodii</dc:creator>
    <dc:date>2016-06-07T11:27:02Z</dc:date>
    <item>
      <title>Can bus clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-bus-clock/m-p/515871#M32619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can bus clock must be based on the bus clock is 50Mhz？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 06:07:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-bus-clock/m-p/515871#M32619</guid>
      <dc:creator>songtao8940</dc:creator>
      <dc:date>2016-06-07T06:07:51Z</dc:date>
    </item>
    <item>
      <title>Re: Can bus clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-bus-clock/m-p/515872#M32620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A CAN interface must be clocked from a accurate source, so 'crystal based', and at a rate AT LEAST 8x bit-rate for 8 quanta (Tq), preferably 16, to place an accurate sample-point 'late' in the bit-cell.&amp;nbsp; In my systems I start with an 8MHz crystal, and I let the CAN clock run directly from /2 of that to make 250kbit/s J1939.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You seem to have a LOT of questions about how to make CAN work.&amp;nbsp; I suggest you look at many of the other recent posts about getting CAN to pass full messages,like this one:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2019" data-containertype="14" data-objectid="394516" data-objecttype="1" href="https://community.nxp.com/thread/394516"&gt;https://community.nxp.com/thread/394516&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CAN peripherals are very sophisticated standalone communication links, but the downside is that everything has to work 'perfectly' about the interchange to get ANY indication of 'communication' to the CPU.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 10:13:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-bus-clock/m-p/515872#M32620</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-06-07T10:13:30Z</dc:date>
    </item>
    <item>
      <title>Re: Can bus clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-bus-clock/m-p/515873#M32621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;first,Thank you for your answer.My can bus part does not work properly with the download function, the communication speed is based on bus clock is 50MHz. Now my bus clock should not 50, I want to know is the 50MHz is not MK20DX128VLH7 this chip the inherent。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 11:24:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-bus-clock/m-p/515873#M32621</guid>
      <dc:creator>songtao8940</dc:creator>
      <dc:date>2016-06-07T11:24:47Z</dc:date>
    </item>
    <item>
      <title>Re: Can bus clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-bus-clock/m-p/515874#M32622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no 'inherent' rate for CPU or Bus clock, there are just 'maximums'.&amp;nbsp; Your general MCG clock setup will determine those.&amp;nbsp; I recommend running the CAN bit-rate-divisor functions directly from the input (XTAL) clock.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 11:27:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-bus-clock/m-p/515874#M32622</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2016-06-07T11:27:02Z</dc:date>
    </item>
    <item>
      <title>Re: Can bus clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-bus-clock/m-p/515875#M32623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,Another problem is just the welded board with downloader not identify them, what way do&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 11:32:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-bus-clock/m-p/515875#M32623</guid>
      <dc:creator>songtao8940</dc:creator>
      <dc:date>2016-06-07T11:32:07Z</dc:date>
    </item>
  </channel>
</rss>