<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K65 fails erase and program at 0x14000 in RUN mode (running with ULINK ICE)</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-fails-erase-and-program-at-0x14000-in-RUN-mode-running-with/m-p/511975#M32388</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Im not using KBOOT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I check that the flash is not over 28Mhz?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The chip is running at 120Mhz (RUN mode) not HSRUN mode&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Apr 2016 13:58:28 GMT</pubDate>
    <dc:creator>steverobalino</dc:creator>
    <dc:date>2016-04-19T13:58:28Z</dc:date>
    <item>
      <title>K65 fails erase and program at 0x14000 in RUN mode (running with ULINK ICE)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-fails-erase-and-program-at-0x14000-in-RUN-mode-running-with/m-p/511973#M32386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Im debugging a bootloader on the K65 tower&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to erase the application space starting at 0x14000 (16K bytes total)&lt;/P&gt;&lt;P&gt;the erase never completes , it resets the MPU?&lt;/P&gt;&lt;P&gt;same thing when I try to program a flash sector&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Im executing: BOARD_BootClockRUN(); ....so the board is running at 120Mhz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know at 180Mhz it wont work, but 120Mhz is OK.?&lt;/P&gt;&lt;P&gt;why would erase and program crash?&lt;/P&gt;&lt;P&gt;when I erase the top of flash...0x1FE000U ...it works fine&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any ideas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Apr 2016 18:43:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-fails-erase-and-program-at-0x14000-in-RUN-mode-running-with/m-p/511973#M32386</guid>
      <dc:creator>steverobalino</dc:creator>
      <dc:date>2016-04-18T18:43:27Z</dc:date>
    </item>
    <item>
      <title>Re: K65 fails erase and program at 0x14000 in RUN mode (running with ULINK ICE)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-fails-erase-and-program-at-0x14000-in-RUN-mode-running-with/m-p/511974#M32387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steven,&lt;/P&gt;&lt;P&gt;After had a brief look through the statement above, I'm still not clear with your issue, so I'd like to get to understand your issue by through these questions below.&lt;/P&gt;&lt;P&gt;1. Did you use the KBOOT bootloader solution?&lt;/P&gt;&lt;P&gt;2. Did the flash clock beyond the 28 Mhz when the MCU works at the 180 MHz?&lt;/P&gt;&lt;P&gt;I'm looking forward to your reply.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2016 10:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-fails-erase-and-program-at-0x14000-in-RUN-mode-running-with/m-p/511974#M32387</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-04-19T10:13:32Z</dc:date>
    </item>
    <item>
      <title>Re: K65 fails erase and program at 0x14000 in RUN mode (running with ULINK ICE)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-fails-erase-and-program-at-0x14000-in-RUN-mode-running-with/m-p/511975#M32388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Im not using KBOOT&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I check that the flash is not over 28Mhz?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The chip is running at 120Mhz (RUN mode) not HSRUN mode&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2016 13:58:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-fails-erase-and-program-at-0x14000-in-RUN-mode-running-with/m-p/511975#M32388</guid>
      <dc:creator>steverobalino</dc:creator>
      <dc:date>2016-04-19T13:58:28Z</dc:date>
    </item>
  </channel>
</rss>