<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TWR-K70F120M CAN Communication  in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-CAN-Communication/m-p/511850#M32375</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Manuel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your question about the CAN transceiver setting, I think this is the configuration for TWR-SER board.&lt;/P&gt;&lt;P&gt;1)you can connect the CAN differential signal to the pin1&amp;amp;3 of J7, pin1 is CANH,pin3 is CANL.&lt;/P&gt;&lt;P&gt;2)regarding the J6 jumper setting, pls close pin1&amp;amp;2, pin 5&amp;amp;6, pin7&amp;amp;8,pin9&amp;amp;10, OPEN 3&amp;amp;4. In the above setting the U4 CAN transceiver woks normally.&lt;/P&gt;&lt;P&gt;For the TWR-K70 board, you should populate the R22 and R33 with&amp;nbsp; low resistors, you should use the CAN1 module, in other words, use the PTC16 as CAN1_RX and PTC17 as CAN1_TX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Mar 2016 06:18:24 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2016-03-30T06:18:24Z</dc:date>
    <item>
      <title>TWR-K70F120M CAN Communication</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-CAN-Communication/m-p/511849#M32374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a TWR-K70F120M with the TWR-SER board and I don't have any signal in the input of CAN TRX. I'm not sure if the connection between thetwo boards is direct or I have to configure or soldier some resistors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Mar 2016 15:47:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-CAN-Communication/m-p/511849#M32374</guid>
      <dc:creator>manolojoaquin</dc:creator>
      <dc:date>2016-03-29T15:47:26Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-K70F120M CAN Communication</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-CAN-Communication/m-p/511850#M32375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Manuel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your question about the CAN transceiver setting, I think this is the configuration for TWR-SER board.&lt;/P&gt;&lt;P&gt;1)you can connect the CAN differential signal to the pin1&amp;amp;3 of J7, pin1 is CANH,pin3 is CANL.&lt;/P&gt;&lt;P&gt;2)regarding the J6 jumper setting, pls close pin1&amp;amp;2, pin 5&amp;amp;6, pin7&amp;amp;8,pin9&amp;amp;10, OPEN 3&amp;amp;4. In the above setting the U4 CAN transceiver woks normally.&lt;/P&gt;&lt;P&gt;For the TWR-K70 board, you should populate the R22 and R33 with&amp;nbsp; low resistors, you should use the CAN1 module, in other words, use the PTC16 as CAN1_RX and PTC17 as CAN1_TX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it can help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Mar 2016 06:18:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K70F120M-CAN-Communication/m-p/511850#M32375</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2016-03-30T06:18:24Z</dc:date>
    </item>
  </channel>
</rss>