<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: [Processor Expert] This interrupt is required/Unassigned peripheral</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Processor-Expert-This-interrupt-is-required-Unassigned/m-p/511247#M32285</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fiona,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the same issue as @William Koos&lt;/P&gt;&lt;P&gt;Could you please give a hand with this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Sep 2016 15:14:00 GMT</pubDate>
    <dc:creator>alubeiro</dc:creator>
    <dc:date>2016-09-19T15:14:00Z</dc:date>
    <item>
      <title>[Processor Expert] This interrupt is required/Unassigned peripheral</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Processor-Expert-This-interrupt-is-required-Unassigned/m-p/511244#M32282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After changing the processor component from a K26 MK26FN2M0CAC18 to MK26FN2M0VMI18, which has the same flash, ram, and number of I/Os, Processor Expert had a few errors. I fixed most of them by specifying the referenced component, but in the `fsl_gpio` component I cannot find a solution to the "PORTC Interrupt" "missing" error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried removing all the components that use PORTC and the GPIO pins on that port. I also tried disabling and re-enabling "Auto initialization" for this component.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to fix it? Or is there a recommend process for changing the processor in a project to avoid these types of errors?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problems are:&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;Description&lt;/TD&gt;&lt;TD&gt;Resource&lt;/TD&gt;&lt;TD&gt;Path&lt;/TD&gt;&lt;TD&gt;Location&lt;/TD&gt;&lt;TD&gt;Type&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;This interrupt is required (Interrupt)&lt;/TD&gt;&lt;TD&gt;project_name&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;gpio1/Interrupt&lt;/TD&gt;&lt;TD&gt;Processor Expert Problem&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;Unassigned peripheral (Device)&lt;/TD&gt;&lt;TD&gt;project_name&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;gpio1/Device&lt;/TD&gt;&lt;TD&gt;Processor Expert Problem&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32486iDD8853233675E71D/image-size/large?v=v2&amp;amp;px=999" title="Selection_014.png" alt="Selection_014.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Apr 2016 18:04:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Processor-Expert-This-interrupt-is-required-Unassigned/m-p/511244#M32282</guid>
      <dc:creator>lucasrangit</dc:creator>
      <dc:date>2016-04-18T18:04:32Z</dc:date>
    </item>
    <item>
      <title>Re: [Processor Expert] This interrupt is required/Unassigned peripheral</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Processor-Expert-This-interrupt-is-required-Unassigned/m-p/511245#M32283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Lucas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;Could you please check whether the PROTC IRQ Handler is enabled under ‘Events’ tab of fsl_gpio component, please see the screenshot as below:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32455i2E2258D55366231A/image-size/large?v=v2&amp;amp;px=999" title="k26gpio1.png" alt="k26gpio1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32496iDD35EC01DCF37C52/image-size/large?v=v2&amp;amp;px=999" title="k26gpio2.png" alt="k26gpio2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Arial','sans-serif';"&gt;If this does not help, could you please attach an example project to help us reproduce the error? Thank you very much!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Fiona Kuang&lt;/P&gt;&lt;P&gt;TIC - Technical Information Center&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Mark Correct button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2016 11:42:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Processor-Expert-This-interrupt-is-required-Unassigned/m-p/511245#M32283</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2016-04-19T11:42:14Z</dc:date>
    </item>
    <item>
      <title>Re: [Processor Expert] This interrupt is required/Unassigned peripheral</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Processor-Expert-This-interrupt-is-required-Unassigned/m-p/511246#M32284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm having the same issue. I'm using KDSK 1.2 and KDS 3.0.0 with Cpu:MK64FN1M0VLQ12. I've been using this project for at least a year. I want to use PTD10 as a input interrupt. As soon as I select "generate code" under the Events tab -&amp;gt; PORTD_IRQ_handler I get an error under the Properties tab -&amp;gt; PORTD_Interrupt in the Device and Interrupt columns. The Device Column error is "ERROR: Unassigned peripheral" but there are no options to select from in the column. Similarly the error in the Interrupt column is "ERROR: This interrupt is required" but there are no options to select from.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37483i12CD1E19E786ED23/image-size/large?v=v2&amp;amp;px=999" title="Screen Shot 2016-07-12 at 9.55.29 AM.png" alt="Screen Shot 2016-07-12 at 9.55.29 AM.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 13:56:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Processor-Expert-This-interrupt-is-required-Unassigned/m-p/511246#M32284</guid>
      <dc:creator>intractablesubt</dc:creator>
      <dc:date>2016-07-12T13:56:34Z</dc:date>
    </item>
    <item>
      <title>Re: [Processor Expert] This interrupt is required/Unassigned peripheral</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Processor-Expert-This-interrupt-is-required-Unassigned/m-p/511247#M32285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fiona,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the same issue as @William Koos&lt;/P&gt;&lt;P&gt;Could you please give a hand with this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2016 15:14:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Processor-Expert-This-interrupt-is-required-Unassigned/m-p/511247#M32285</guid>
      <dc:creator>alubeiro</dc:creator>
      <dc:date>2016-09-19T15:14:00Z</dc:date>
    </item>
  </channel>
</rss>