<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Timer and interrupt</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Timer-and-interrupt/m-p/206607#M3221</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;P&gt;I'm not sure how to integrate the code you've posted into my environment.&lt;/P&gt;&lt;P&gt;I'm using &lt;U&gt;&lt;STRONG&gt;uVision 4 IDE&lt;/STRONG&gt;&lt;/U&gt;, &amp;nbsp;the only include file I have is "&lt;U&gt;&lt;STRONG&gt;MK60N512MD100.h&lt;/STRONG&gt;&lt;/U&gt;", it's a basic CMSIS style interface to the K60&amp;nbsp; that was created by Freescale. None of your defines are recognized in this header and I'm not&lt;/P&gt;&lt;P&gt;&amp;nbsp;sure how to proceed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Eitan.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 May 2011 15:36:17 GMT</pubDate>
    <dc:creator>eitanm</dc:creator>
    <dc:date>2011-05-16T15:36:17Z</dc:date>
    <item>
      <title>Timer and interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Timer-and-interrupt/m-p/206605#M3219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="MsoNormal"&gt;Hi, the following will be the first of possibly&amp;nbsp;many questions I'm going to post here,&lt;/P&gt;&lt;P class="MsoNormal"&gt;Sorry in advance for the noob&amp;nbsp;nature of those questions. If there is a good documentation (other then the reference manual) feel free to kindly point me there.&lt;/P&gt;&lt;P class="MsoNormal"&gt;I'm attempting to make my first steps with the Tower K60, I'm working with &lt;STRONG&gt;uvision\Keil IDE&lt;/STRONG&gt; (so no CodeWarrior, and no MQX), all I have is&amp;nbsp;a&amp;nbsp;working Blinky sample..&lt;/P&gt;&lt;P class="MsoNormal"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="MsoNormal"&gt;1. How do I configure the&amp;nbsp;interrupt vector table? I went through ARM's CMSIS NVIC interface, I could not find how-to install a function pointer to be execute on an interrupt event.&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN style="mso-spacerun: yes;"&gt;&amp;nbsp;&lt;/SPAN&gt;2. How do I set a simple timer (I guess PIT ?) to trigger my interrupt handler.&lt;/P&gt;&lt;P class="MsoNormal"&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="MsoNormal"&gt;Thanks,&lt;/P&gt;&lt;P class="MsoNormal"&gt;Eitan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 15 May 2011 20:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Timer-and-interrupt/m-p/206605#M3219</guid>
      <dc:creator>eitanm</dc:creator>
      <dc:date>2011-05-15T20:27:28Z</dc:date>
    </item>
    <item>
      <title>Re: Timer and interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Timer-and-interrupt/m-p/206606#M3220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Assuming interrup vectors in RAM:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Cortex M4 core's vector table offset needs to be configured, eg.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;VECTOR_TABLE_OFFSET_REG&amp;nbsp;&amp;nbsp; = (RAM_START_ADDRESS);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // position the vector table at the bottom of RAM&lt;/STRONG&gt;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The interrupt needs to be entered into the table and the Cortex NVIC registers configured with the interrupt's priority and enabled, eg.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;// Function used to enter processor interrupts&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;//&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;static void fnEnterInterrupt(int iInterruptID, unsigned char ucPriority, void (*InterruptFunc)(void))&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;{&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; unsigned long *ptrIntSet = IRQ0_31_SER_ADD;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; unsigned char *ptrPriority = IRQ0_3_PRIORITY_REGISTER_ADD;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; VECTOR_TABLE *ptrVect;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; void ( **processor_ints )( void );&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ptrVect = (VECTOR_TABLE *)(RAM_START_ADDRESS);&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; processor_ints = (void (**)(void))&amp;amp;ptrVect-&amp;gt;processor_interrupts;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; processor_ints += iInterruptID;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; *processor_ints = InterruptFunc;&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ptrIntSet += (iInterruptID/32);&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; *ptrIntSet = (0x01 &amp;lt;&amp;lt; (iInterruptID%32));&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // enable the interrupt&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ptrPriority += iInterruptID;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; *ptrPriority = ucPriority;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // define the interrupt's priority&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;}﻿&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Usually the Cortex M4's SYSTICK is used as tick timer (this leaves PITs free for other functions).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, to configure a PIT0 interrupt the following can be done:&lt;/P&gt;&lt;P&gt;1) Enable clocks to the PIT0 module [&lt;STRONG&gt;SIM_SCG6 |= (SIM_SCGC6_PIT﻿);&lt;/STRONG&gt;﻿]&lt;/P&gt;&lt;P&gt;2) Enter the PIT handler [&lt;STRONG&gt;fnEnterInterrupt(irq_PIT0_ID, PIT_int_priority, _PIT0_Interrupt);&lt;/STRONG&gt;﻿]&lt;/P&gt;&lt;P&gt;3) Configure and start the PIT0 (see data sheet)&lt;/P&gt;&lt;P&gt;4) Handle the interrupt, eg:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;STRONG&gt;static __interrupt void _PIT0_Interrupt(void)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;{&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PIT_TFLG0 = PIT_TFLG_TIF;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // clear pending interrupts&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; ... other stuff&lt;BR /&gt;&lt;STRONG&gt;}﻿&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are various additional developer's tips in the following document - see the appendix: &lt;A href="http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf%FEFF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/KINETIS/uTaskerV1.4_Kinetis_demo.pdf﻿&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 May 2011 01:24:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Timer-and-interrupt/m-p/206606#M3220</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-05-16T01:24:31Z</dc:date>
    </item>
    <item>
      <title>Re: Timer and interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Timer-and-interrupt/m-p/206607#M3221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;P&gt;I'm not sure how to integrate the code you've posted into my environment.&lt;/P&gt;&lt;P&gt;I'm using &lt;U&gt;&lt;STRONG&gt;uVision 4 IDE&lt;/STRONG&gt;&lt;/U&gt;, &amp;nbsp;the only include file I have is "&lt;U&gt;&lt;STRONG&gt;MK60N512MD100.h&lt;/STRONG&gt;&lt;/U&gt;", it's a basic CMSIS style interface to the K60&amp;nbsp; that was created by Freescale. None of your defines are recognized in this header and I'm not&lt;/P&gt;&lt;P&gt;&amp;nbsp;sure how to proceed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Eitan.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 May 2011 15:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Timer-and-interrupt/m-p/206607#M3221</guid>
      <dc:creator>eitanm</dc:creator>
      <dc:date>2011-05-16T15:36:17Z</dc:date>
    </item>
    <item>
      <title>Re: Timer and interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Timer-and-interrupt/m-p/206608#M3222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Eitan&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have attached the header file that the above code uses - you can look up the defines there and exchange for the defines in your file if you want.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Additional project defines for the chip type used are (with 512k FLASH):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define SIZE_OF_FLASH&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (512*1024)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // 512k FLASH&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define SIZE_OF_RAM&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (128 * 1024)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // 128k SRAM﻿&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Alternatively you can get the complete project (including uVision project) from the uTasker web site (&lt;A href="http://www.uTasker.com" rel="nofollow" target="_self"&gt;http://www.uTasker.com&lt;/A&gt;) - this allows simulation of the Kinetis device, including simulation of the interrupt mechanisms, thus simplifying first steps as well as complete projects.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 May 2011 18:38:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Timer-and-interrupt/m-p/206608#M3222</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-05-16T18:38:39Z</dc:date>
    </item>
  </channel>
</rss>