<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FRDM-KL25Z battery power problem</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509890#M32168</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Curioser and curioser.&amp;nbsp; Since the board works with the KL25Z-USB connection the DC-DC converter is working.&amp;nbsp; Also, the 3.3v input bypasses the converter.&amp;nbsp; I tried powering the board using a USB charger and the KL25Z-USB connection.&amp;nbsp; No Luck!&amp;nbsp; It appears that the USB library I'm using may be the problem.&amp;nbsp; If it cannot initialise, it hangs.&amp;nbsp; I think.&amp;nbsp; I'm using the online mbed IDE.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Feb 2016 05:15:11 GMT</pubDate>
    <dc:creator>bobalong</dc:creator>
    <dc:date>2016-02-16T05:15:11Z</dc:date>
    <item>
      <title>FRDM-KL25Z battery power problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509886#M32164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My project is a simple timestamp logger.&amp;nbsp; I'm using a FRDM-KL25Z with&amp;nbsp; a DS3231 I2C clock module, and 2 buttons with 22K pullups.&amp;nbsp; I assume I have a Rev-D board since there is no provision on board for a 5v regulator and associated caps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It works well when connected to my PC using the KL25Z-USB connector, but not when using the other supply options.&amp;nbsp; I have tried regulated 5v on VIN and regulated 3.3 v on the 3.3v pin.&amp;nbsp; The program does not work with either.&amp;nbsp; Both behave the same as when I use the OpenSDA connector ( which I know does not allow the program to run).&amp;nbsp; I have not tried attaching a coin cell yet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I power the project with a battery?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 14 Feb 2016 13:02:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509886#M32164</guid>
      <dc:creator>bobalong</dc:creator>
      <dc:date>2016-02-14T13:02:25Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z battery power problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509887#M32165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James,&lt;/P&gt;&lt;P&gt;the usual way is to connect your battery to V_IN. This is what I'm using (see &lt;A href="http://mcuoneclipse.com/2013/06/21/5v-generation-from-v_in-on-the-freedom-board-reve/" title="http://mcuoneclipse.com/2013/06/21/5v-generation-from-v_in-on-the-freedom-board-reve/"&gt;5V Generation from V_IN on the Freedom Board RevE | MCU on Eclipse&lt;/A&gt; ). However, if you need 5V on the 5V header, then you need to add a DC-DC converter (see that article) to generate 5V from V_IN, as this is otherwise generated from the USB connector (check the board schematics).&lt;/P&gt;&lt;P&gt;I assume that you have your DS3231 (or 3232?) powered by 3.3V, so you should be fine. But if you have other (off-board) peripherals, you need to generate that 5V from the battery somehow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Feb 2016 07:15:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509887#M32165</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-02-15T07:15:49Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z battery power problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509888#M32166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately, no help.&amp;nbsp; I do not need 5v, only 3.3v.&amp;nbsp; The only reason I tried 5v was to see if it would work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I said before, connecting the proper voltage supply to the VIN and 3.3v pins does not work.&amp;nbsp; I have tried with 2 boards with the same result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any clues on where to get a coin-cell holder for the board?&amp;nbsp; All the ones I've seen do not have compatible pins.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Feb 2016 11:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509888#M32166</guid>
      <dc:creator>bobalong</dc:creator>
      <dc:date>2016-02-15T11:18:34Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z battery power problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509889#M32167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi James,&lt;/P&gt;&lt;P&gt;I suggest you check the schematics as it could be that you have damaged the DC-DC converters somehow? Follow the path on the schematics and check if the parts have the proper voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the con cell holder: &lt;A href="http://mcuoneclipse.com/2012/10/23/completing-the-frdm-kl25z-board/" title="http://mcuoneclipse.com/2012/10/23/completing-the-frdm-kl25z-board/"&gt;Completing the FRDM-KL25Z Board | MCU on Eclipse&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Feb 2016 11:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509889#M32167</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2016-02-15T11:33:45Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z battery power problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509890#M32168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Curioser and curioser.&amp;nbsp; Since the board works with the KL25Z-USB connection the DC-DC converter is working.&amp;nbsp; Also, the 3.3v input bypasses the converter.&amp;nbsp; I tried powering the board using a USB charger and the KL25Z-USB connection.&amp;nbsp; No Luck!&amp;nbsp; It appears that the USB library I'm using may be the problem.&amp;nbsp; If it cannot initialise, it hangs.&amp;nbsp; I think.&amp;nbsp; I'm using the online mbed IDE.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Feb 2016 05:15:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509890#M32168</guid>
      <dc:creator>bobalong</dc:creator>
      <dc:date>2016-02-16T05:15:11Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL25Z battery power problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509891#M32169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was barking up&amp;nbsp; the wrong tree!&amp;nbsp; It was a USB issue, not power.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The project is a pocket-size device that will log the time each time a button is pressed.&amp;nbsp; At the end of the day it will bit connected via USB to my PC to upload the results.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had the USBKeyboard declaration at the top of the code, so the USB initialisation occurred long before it was needed. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I moved it into the function that does the transfer with a 2 second delay after it and the project works as intended.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Feb 2016 06:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KL25Z-battery-power-problem/m-p/509891#M32169</guid>
      <dc:creator>bobalong</dc:creator>
      <dc:date>2016-02-16T06:17:39Z</dc:date>
    </item>
  </channel>
</rss>