<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックConnect NAND Flash by FlexBus</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-NAND-Flash-by-FlexBus/m-p/509882#M32162</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use K61 and K70 in our products now. I want to use the K65 in our new projects since it offers higher Flash and SRAM. I noticed the new Kinetis' has no NAND Flash Controller. Is it possible to connect NAND Flash via FlexBus?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Dec 2015 06:55:12 GMT</pubDate>
    <dc:creator>Austin</dc:creator>
    <dc:date>2015-12-30T06:55:12Z</dc:date>
    <item>
      <title>Connect NAND Flash by FlexBus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-NAND-Flash-by-FlexBus/m-p/509882#M32162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use K61 and K70 in our products now. I want to use the K65 in our new projects since it offers higher Flash and SRAM. I noticed the new Kinetis' has no NAND Flash Controller. Is it possible to connect NAND Flash via FlexBus?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Dec 2015 06:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-NAND-Flash-by-FlexBus/m-p/509882#M32162</guid>
      <dc:creator>Austin</dc:creator>
      <dc:date>2015-12-30T06:55:12Z</dc:date>
    </item>
    <item>
      <title>Re: Connect NAND Flash by FlexBus</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-NAND-Flash-by-FlexBus/m-p/509883#M32163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Austin,&lt;/P&gt;&lt;P&gt;It's possible to connect the NAND Flash directly by using the Flexbus interface, however it's not very usual and simple.&lt;/P&gt;&lt;P&gt;The problem is the NAND flash is block oriented and need some software error corrections.So it means that system needs software driver which takes care about this.&lt;/P&gt;&lt;P&gt;But we don't have such standalone driver for this now.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jan 2016 03:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Connect-NAND-Flash-by-FlexBus/m-p/509883#M32163</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-01-04T03:24:49Z</dc:date>
    </item>
  </channel>
</rss>