<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Peripheral Chip Select on K22</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Peripheral-Chip-Select-on-K22/m-p/509818#M32156</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K22 has two different SPI interfaces, one with 1 deep FIFO and 1 with 4 byte deep FIFO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using the 4 deep FIFO it is possible to program the behaviour of the CS for each byte prepared - in case of the single depth FIFO this is not an option so the advantage is not the same on all SPI instances - &lt;EM&gt;one needs to be careful since the driver of each may need to be different!&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using CS peripheral lines it is also possible to specifiy some timing behavior so that there is a certain delay before or after data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In most cases it is however just as easy (and sometimes easier) to control them with a port output instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Dec 2015 05:24:56 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2015-12-30T05:24:56Z</dc:date>
    <item>
      <title>Peripheral Chip Select on K22</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Peripheral-Chip-Select-on-K22/m-p/509817#M32155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How are the Peripheral Chip Select pins different than just taking a normal digital out and using that as a chip select?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Dec 2015 02:35:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Peripheral-Chip-Select-on-K22/m-p/509817#M32155</guid>
      <dc:creator>gibson486</dc:creator>
      <dc:date>2015-12-30T02:35:42Z</dc:date>
    </item>
    <item>
      <title>Re: Peripheral Chip Select on K22</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Peripheral-Chip-Select-on-K22/m-p/509818#M32156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K22 has two different SPI interfaces, one with 1 deep FIFO and 1 with 4 byte deep FIFO.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using the 4 deep FIFO it is possible to program the behaviour of the CS for each byte prepared - in case of the single depth FIFO this is not an option so the advantage is not the same on all SPI instances - &lt;EM&gt;one needs to be careful since the driver of each may need to be different!&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using CS peripheral lines it is also possible to specifiy some timing behavior so that there is a certain delay before or after data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In most cases it is however just as easy (and sometimes easier) to control them with a port output instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Dec 2015 05:24:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Peripheral-Chip-Select-on-K22/m-p/509818#M32156</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-12-30T05:24:56Z</dc:date>
    </item>
    <item>
      <title>Re: Peripheral Chip Select on K22</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Peripheral-Chip-Select-on-K22/m-p/509819#M32157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Andrew Chin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Do you mean you want to use the GPIO in K22&amp;nbsp; as the peripheral chip select pins? Or the module's pin in the K22, if it is the module's pin, which module you are using?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you just use the GPIO, you need&amp;nbsp; check the IO current driver ability, whether it is enough to driver your peripheral chip, more details, please refer to the K22 datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact me!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Dec 2015 06:35:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Peripheral-Chip-Select-on-K22/m-p/509819#M32157</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-12-30T06:35:07Z</dc:date>
    </item>
  </channel>
</rss>