<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K60 RTC VBAT Current Draw in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509695#M32142</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Circuit tested shown below.&lt;/P&gt;&lt;P&gt;D8 pin6 is normally connected to VDD_BB but was removed to eliminate any reverse leakage current error term.&lt;/P&gt;&lt;P&gt;Voltage was measured across R260 to determine IDD_VBAT.&lt;/P&gt;&lt;P&gt;External power supply was placed across C7 to check IDD_VAT at 3.0V and 1.8V.&lt;/P&gt;&lt;P&gt;3.3V was power supply was shut down (VCC ≈ 0V).&lt;/P&gt;&lt;P&gt;Unit was otherwise isolated in environmental chamber.&lt;/P&gt;&lt;P&gt;(Note: CU6L6 is ceramic capacitor (low leakage). Removed CU6L6 on one control and verified  it had no effect.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 May 2016 15:19:01 GMT</pubDate>
    <dc:creator>danielwaser</dc:creator>
    <dc:date>2016-05-05T15:19:01Z</dc:date>
    <item>
      <title>K60 RTC VBAT Current Draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509687#M32134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am designing with a MK66FN2M0VMD18 microcontroller and using the RTC circuitry with VBAT power supplied through an external Supercap. I have an external 32.768Khz crystal oscillator for the RTC&amp;nbsp; which uses the internal tunable capacitors configurable by software. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RTC is configured to use the RTC Alarm output (RTC_WAKEUP_B) to turn on the power supply (required function if power supply is present) and the RTC_CLKOUT pin is also enabled to output the 32.768Khz clock (optional used to monitor/test).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;VBAT is powered to approximately 3.0V through diode from 3.3VCC when power is active.&lt;/P&gt;&lt;P&gt;Design intent to is have RTC maintain time when power is OFF for up to 72 hours over operating temp of -40C to +85C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I looked at the Data sheet and User Guide to try to understand the current draw specifications and would like the current draw clarified.&lt;/P&gt;&lt;P&gt;In Section 2.2.4 Power Mode Transition Operating Behaviors Table 6, it states that IRTC (typ) current draw varies from 357-810 nA -40C to 105C) in VLLS1 mode.&lt;/P&gt;&lt;P&gt;In Section 2.2.5 Power Consumption Operating Behaviors Table 7, it states IDD_VBAT (avg) when CPU is not accessing RTC registers is 6.33uA (at 105C) to 0.8uA (from -40C to 25C) for VBAT = 3.0V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From description it is not clear to me what the VBAT current draw is when the micro is otherwise unpowered in order to size the appropriate backup power source (supercap) for 72 hour backup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My questions are:&lt;/P&gt;&lt;P&gt;1. What is worst case IDD_VBAT when VCC is 0V (-40C to +85C)?&lt;/P&gt;&lt;P&gt;2. Does use of RTC_WAKEUP or RTC_CLKOUT affect the IDD_VBAT current draw when VCC = 0V?&lt;/P&gt;&lt;P&gt;3. Do any RTC resister settings affect the current draw of module when VCC = 0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Apr 2016 16:34:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509687#M32134</guid>
      <dc:creator>danielwaser</dc:creator>
      <dc:date>2016-04-15T16:34:42Z</dc:date>
    </item>
    <item>
      <title>Re: K60 RTC VBAT Current Draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509688#M32135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/karinavalencia"&gt;karinavalencia&lt;/A&gt;​,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I've looked thru the K66 datasheet and also AN4503_Kinetis Power Management app note on behalf of my customer (Dan Waser), and determined that the values Dan is seeking are not specified in either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The app note and datasheet only mention that the IDD_VBAT value can increase when the VBAT registers are being accessed by the CPU,&amp;nbsp; but does not mention any other potential adders, such as when using RTC_CLKOUT or RTC_WAKEUP.&amp;nbsp; So it appears these do not cause an increase in IDD_VBAT and its fairly isolated from the main power supply, but confirmation would help Dan greatly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Bottom line, Dan would like to power his product for 72 hours using a SuperCap, and clarifying the worse case IDD_VBAT value and any potential adders will help him pick the correct SuperCap value to enable this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Gordy Carlson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2016 18:51:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509688#M32135</guid>
      <dc:creator>GordyCarlson</dc:creator>
      <dc:date>2016-04-19T18:51:33Z</dc:date>
    </item>
    <item>
      <title>Re: K60 RTC VBAT Current Draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509689#M32136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dan and Gordy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think there are a few misunderstandings about the RTC and VBAT that are muddying the waters here. I'd like to start with a bit of information...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RTC_CLKOUT pin is actually in the main VDD domain, the pin is NOT in the VBAT domain. So you should know that RTC_CLKOUT will not toggle if the main VDD =0. RTC_CLKOUT also goes away in some of the low power modes. Because RTC_CLKOUT is in the digital domain, enabling that pin function doesn't affect VBAT current draw (although enabling the oscillator and the RTC itself does as that is all in the VBAT domain).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also the VBAT domain is a completely isolated domain. There isn't any internal switching so that VBAT is powered from the main when it is available, so for a given RTC configuration and temp VBAT current draw should be fairly stable and doesn't vary based on what is happening with VDD or the power mode of the CPU. The exception is when the core is accessing RTC registers as that generates activity in the VBAT domain.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To answer your questions now...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. The second set of IDD_VBAT specs in Table 7 are what you want. This is with the RTC and 32kHz osc enabled which sounds like the configuration you will be using. You can't access the registers using the CPU if VDD=0, so this spec covers the VDD=0 case.&lt;/P&gt;&lt;P&gt;2. Not much. As I described above, RTC_CLKOUT is not in the VBAT domain, so it doesn't affect current draw. RTC_WAKEUP is&amp;nbsp; an active low, open drain pin so it won't cause the normal state current to go up if enabled. You'll get a slight bump when the pin asserts based on the pullup resistor value and loading on the pin.&lt;/P&gt;&lt;P&gt;3. I'm not quite sure how to answer this one. If you don't have the RTC enabled, then that would definitely decrease current, but you want to use it, so I don't think that is what you are asking. I guess I can say that the current draw when VDD is powered shouldn't be different than when VDD=0. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Melissa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2016 14:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509689#M32136</guid>
      <dc:creator>melissa_hunter</dc:creator>
      <dc:date>2016-04-22T14:23:33Z</dc:date>
    </item>
    <item>
      <title>Re: K60 RTC VBAT Current Draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509690#M32137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank You Melissa!&amp;nbsp; I suspected RTC_CLKOUT was completely in the VDD domain,&amp;nbsp; great to get a confirmation that it does not impact IDD_VBAT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Gordy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 18:49:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509690#M32137</guid>
      <dc:creator>GordyCarlson</dc:creator>
      <dc:date>2016-04-26T18:49:48Z</dc:date>
    </item>
    <item>
      <title>Re: K60 RTC VBAT Current Draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509691#M32138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Melissa,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Dan asks for clarification on what the IDD_Vbat is....&amp;nbsp; here is a cut/paste of the email response he provided me...&lt;/P&gt;&lt;P&gt;My take on this is that 810na I_RTC value is an adder to the main rail power consumption when the RTC is enabled, and that IDD_Vbat of 0.8ua to 6.33ua over temp is the correct answer.&amp;nbsp; Confirmation appreciated. Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;" &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;Still not sure what current max draw to expect from IDD_VBAT over temp when VC C =0V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;&amp;nbsp; In Section 2.2.4 Power Mode Transition Operating Behaviors Table 6, it states that IRTC (typ) current draw varies from 357 to 810 nA -40C to 105C) in VLLS1 mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;&amp;nbsp; In Section 2.2.5 Power Consumption Operating Behaviors Table 7, it states IDD_VBAT (avg) when CPU is not accessing RTC registers is 6.33uA (at 105C) to 0.8uA (from -40C to 25C) for VBAT = 3.0V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;Is answer 810nA or 6.33 µA?"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Apr 2016 21:52:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509691#M32138</guid>
      <dc:creator>GordyCarlson</dc:creator>
      <dc:date>2016-04-29T21:52:07Z</dc:date>
    </item>
    <item>
      <title>Re: K60 RTC VBAT Current Draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509692#M32139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gordy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Table 7 are the specs he wants. You're right, table 6 is an adder on the main supply when the RTC is enabled. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Melissa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 May 2016 13:10:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509692#M32139</guid>
      <dc:creator>melissa_hunter</dc:creator>
      <dc:date>2016-05-02T13:10:22Z</dc:date>
    </item>
    <item>
      <title>Re: K60 RTC VBAT Current Draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509693#M32140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-top: auto; margin-bottom: auto;"&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;Dan is still seeing higher IDD_VBAT than expected, in excess of datasheet specs at high temp....he tested four units for IDD_VBAT with VCC = 0 and is finding current draw greater than the max listed in Table 7 of the data sheet.&amp;nbsp; The control’s circuit was changed to just have resistor between VBAT and VBB pin of K66 to make current draw easier to measure. Voltage was measured across resistor to calculate current.&amp;nbsp;&amp;nbsp;&amp;nbsp; See attachment.&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-top: auto; margin-bottom: auto;"&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;The IC marking is:&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-top: auto; margin-bottom: auto;"&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;MK66FN2M0VMD18&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-top: auto; margin-bottom: auto;"&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;0N65N&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-top: auto; margin-bottom: auto;"&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;CTAD1530E&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-top: auto; margin-bottom: auto;"&gt;&lt;/P&gt;&lt;P style="margin-top: auto; margin-bottom: auto;"&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;==================================&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-top: auto; margin-bottom: auto;"&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;Test data over temp with VBB = 1.8V and 3.0V&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-top: auto; margin-bottom: auto;"&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;(Measured values attached as jpg)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I checked the errata for the ON65N mask,&amp;nbsp; there is an errata general power consumption at low temps for "some parts", but nothing noted for issues with IDD_VBAT.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 May 2016 20:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509693#M32140</guid>
      <dc:creator>GordyCarlson</dc:creator>
      <dc:date>2016-05-04T20:52:19Z</dc:date>
    </item>
    <item>
      <title>Re: K60 RTC VBAT Current Draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509694#M32141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gordy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are they collecting these numbers on their own hardware?&amp;nbsp; Could I see the schematic? In particular I would like to see how they are connecting the VBAT domain to the main VDD supply (assuming this is what they are doing to charge up the supercap).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Melissa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 May 2016 14:06:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509694#M32141</guid>
      <dc:creator>melissa_hunter</dc:creator>
      <dc:date>2016-05-05T14:06:25Z</dc:date>
    </item>
    <item>
      <title>Re: K60 RTC VBAT Current Draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509695#M32142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Circuit tested shown below.&lt;/P&gt;&lt;P&gt;D8 pin6 is normally connected to VDD_BB but was removed to eliminate any reverse leakage current error term.&lt;/P&gt;&lt;P&gt;Voltage was measured across R260 to determine IDD_VBAT.&lt;/P&gt;&lt;P&gt;External power supply was placed across C7 to check IDD_VAT at 3.0V and 1.8V.&lt;/P&gt;&lt;P&gt;3.3V was power supply was shut down (VCC ≈ 0V).&lt;/P&gt;&lt;P&gt;Unit was otherwise isolated in environmental chamber.&lt;/P&gt;&lt;P&gt;(Note: CU6L6 is ceramic capacitor (low leakage). Removed CU6L6 on one control and verified  it had no effect.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 May 2016 15:19:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509695#M32142</guid>
      <dc:creator>danielwaser</dc:creator>
      <dc:date>2016-05-05T15:19:01Z</dc:date>
    </item>
    <item>
      <title>Re: K60 RTC VBAT Current Draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509696#M32143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dan replied to the thread email notification with the below info, ....but just in case, attached is a copy of that part of the schematic along with his description below...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;--------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;Circuit tested shown below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;D8 pin6 is normally connected to VDD_BB but was removed to eliminate any reverse leakage current error term. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;Voltage was measured across R260 to determine IDD_VBAT.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;External power supply was placed across C7 to check IDD_VAT at 3.0V and 1.8V. &lt;/SPAN&gt;&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;3.3V was power supply was shut down (VCC ≈ 0V). &lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;Unit was otherwise isolated in environmental chamber.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri',sans-serif; color: #1f497d;"&gt;(Note: CU6L6 is ceramic capacitor (low leakage). Removed CU6L6 on one control and verified&amp;nbsp; it had no effect.)&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;--------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 May 2016 15:36:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509696#M32143</guid>
      <dc:creator>GordyCarlson</dc:creator>
      <dc:date>2016-05-05T15:36:22Z</dc:date>
    </item>
    <item>
      <title>Re: K60 RTC VBAT Current Draw</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509697#M32144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For testing purposes could you try removing D8 from one of the boards. That would completely eliminate the potential for leakage back to the VDD domain.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Melissa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 May 2016 14:42:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-RTC-VBAT-Current-Draw/m-p/509697#M32144</guid>
      <dc:creator>melissa_hunter</dc:creator>
      <dc:date>2016-05-06T14:42:10Z</dc:date>
    </item>
  </channel>
</rss>