<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Fault input disable FTM output for KV11 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fault-input-disable-FTM-output-for-KV11/m-p/508394#M32003</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Original Content posted by Li Yang&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For KV11, the fault input is used for disable PWM output, could you help answer the following two questions?&lt;/P&gt;&lt;P&gt;1. If FTM0_FLT0 is enabled, all channels of FTM0 output are disabled or only FTM0_CH0/FTM0_CH1 are disabled?&lt;/P&gt;&lt;P&gt;2. Whether FTM1_FLT0 can be used to disable PWM output of FTM0_CH0/FTM0_CH1?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;note:&lt;/P&gt;&lt;P&gt;The customer name is Suzhou Norlha, the project is electric wheelchair.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Dec 2015 15:32:40 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2015-12-28T15:32:40Z</dc:date>
    <item>
      <title>Fault input disable FTM output for KV11</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fault-input-disable-FTM-output-for-KV11/m-p/508394#M32003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Original Content posted by Li Yang&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For KV11, the fault input is used for disable PWM output, could you help answer the following two questions?&lt;/P&gt;&lt;P&gt;1. If FTM0_FLT0 is enabled, all channels of FTM0 output are disabled or only FTM0_CH0/FTM0_CH1 are disabled?&lt;/P&gt;&lt;P&gt;2. Whether FTM1_FLT0 can be used to disable PWM output of FTM0_CH0/FTM0_CH1?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;note:&lt;/P&gt;&lt;P&gt;The customer name is Suzhou Norlha, the project is electric wheelchair.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Dec 2015 15:32:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fault-input-disable-FTM-output-for-KV11/m-p/508394#M32003</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2015-12-28T15:32:40Z</dc:date>
    </item>
    <item>
      <title>Re: Fault input disable FTM output for KV11</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fault-input-disable-FTM-output-for-KV11/m-p/508395#M32004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Li Yang,&lt;/P&gt;&lt;P&gt;According to the reference manual, there are two group of bits for configuring the fault control feature of channels.&lt;/P&gt;&lt;P&gt;The FAULTM[1:0] is used to configure the general fault control mode, and the FAULTENn bit is used to enable or disable the fault control feature of the specific pair of the channels.&lt;/P&gt;&lt;P&gt;So it's available to enable one pair of channels in the FTM module.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Dec 2015 03:18:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Fault-input-disable-FTM-output-for-KV11/m-p/508395#M32004</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-12-29T03:18:08Z</dc:date>
    </item>
  </channel>
</rss>