<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How fast resolution could I get using 12 bit ADC? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-fast-resolution-could-I-get-using-12-bit-ADC/m-p/206073#M3185</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How fast could I get the ADC conversion time from 1800 sensor using 60 GPIO pins and 30 ADC pins?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sensing analog signal from 1800 points using 12bit ADC in MK60DN512ZVLQ10 Microcontroller.&lt;/P&gt;&lt;P&gt;It takes little over 170ms now, but from the datasheet Min 20 Ksps(1800 / 20 K = 90ms) ~ Max 818.330 Ksps(1800 / 818.330 K = 2.2ms).&lt;/P&gt;&lt;P&gt;I am using MQX too.&lt;/P&gt;&lt;P&gt;I need 5 ms resolution. Is is possible to get the result with MK60DN512ZVLQ10?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not, do you have other microcontroller to get this resolution?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Oct 2012 18:04:36 GMT</pubDate>
    <dc:creator>jayy</dc:creator>
    <dc:date>2012-10-01T18:04:36Z</dc:date>
    <item>
      <title>How fast resolution could I get using 12 bit ADC?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-fast-resolution-could-I-get-using-12-bit-ADC/m-p/206073#M3185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How fast could I get the ADC conversion time from 1800 sensor using 60 GPIO pins and 30 ADC pins?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sensing analog signal from 1800 points using 12bit ADC in MK60DN512ZVLQ10 Microcontroller.&lt;/P&gt;&lt;P&gt;It takes little over 170ms now, but from the datasheet Min 20 Ksps(1800 / 20 K = 90ms) ~ Max 818.330 Ksps(1800 / 818.330 K = 2.2ms).&lt;/P&gt;&lt;P&gt;I am using MQX too.&lt;/P&gt;&lt;P&gt;I need 5 ms resolution. Is is possible to get the result with MK60DN512ZVLQ10?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not, do you have other microcontroller to get this resolution?&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Oct 2012 18:04:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-fast-resolution-could-I-get-using-12-bit-ADC/m-p/206073#M3185</guid>
      <dc:creator>jayy</dc:creator>
      <dc:date>2012-10-01T18:04:36Z</dc:date>
    </item>
    <item>
      <title>Re: How fast resolution could I get using 12 bit ADC?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-fast-resolution-could-I-get-using-12-bit-ADC/m-p/206074#M3186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jayy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First I'd like to know a couple of things about your project:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) If you sampling1,800 different sensors sensors,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; How are you reading all of them using only 30 ADC channels?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; How are you multiplexing the signals?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) If you are indeed multiplexing the signals you must take into consideration there will be a delay between readings,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; slowing down the total mount of time necessary to perform the readings and conversions&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3 If you are reading 1,800 consecutive samples instead of reading 1,800 different signals you can easily get the &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; conversion time you are looking for, please ellaborate, your statement is not clear enough.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2012 17:19:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-fast-resolution-could-I-get-using-12-bit-ADC/m-p/206074#M3186</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2012-10-31T17:19:53Z</dc:date>
    </item>
  </channel>
</rss>