<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: USB MSD host on TWR-K65F180M</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506879#M31831</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had this issue to, I assume that debug session is halted because when disconnecting all J23 jumpers (regulator inputs) the USB regulator output voltage is not provided. J9 7-8 source the regulator output to MCU. So with this connection scheme there is no power for MCU!. You can connect J23 1-2 or 3-4 and J9 7-8 when you want to power the mcu only from USB and not from external sources.&lt;BR /&gt;And at last I'm sorry for the wrong function name. That applies for SDK 1.0. For SDK 2.0 it may be equivalent if a function USB_HostInit return success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Lenka Polaskova&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Feb 2016 08:09:42 GMT</pubDate>
    <dc:creator>lepol</dc:creator>
    <dc:date>2016-02-25T08:09:42Z</dc:date>
    <item>
      <title>USB MSD host on TWR-K65F180M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506874#M31826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a TWR-K65F180M, and I am trying to run a variation of the usbdisk demo (USB host for a mass storage device, e.g. thumb drive). However, I don't get anything out of the microUSB port (J15).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am guessing the issue is that the microUSB port is not supplying power to peripherals. (When I plug in a basic USB laser mouse, the laser doesn't turn on.) There is a jumper (J13) for enabling/disabling power to the microUSB, but I do have it set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there some other jumper configuration that I need to change to use the microUSB in host mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I have all the jumpers in the default positions except J9 has both 3-4 and 5-6. I've tried varying some of the ones related to the microUSB port, but without any success.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jan 2016 00:35:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506874#M31826</guid>
      <dc:creator>acampbell</dc:creator>
      <dc:date>2016-01-22T00:35:15Z</dc:date>
    </item>
    <item>
      <title>Re: USB MSD host on TWR-K65F180M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506875#M31827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Aaron,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please, can you check which version of board you use and also whether you use USB high speed or full speed in project? &lt;/P&gt;&lt;P&gt;By default, you need to enable power by shorting J13 1-2 and power is provided by digital pin, usually PTD8 (which must be set to logical 1 in project). Could you also measure whether power is provided at USB micro or J13? Could you also insert a breakpoint to a function usb_host_dev_mng_check_configuration attach a device and see what happen?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;&lt;SPAN style="line-height: 1.5;"&gt;Lenka Polaskova&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jan 2016 09:52:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506875#M31827</guid>
      <dc:creator>lepol</dc:creator>
      <dc:date>2016-01-22T09:52:59Z</dc:date>
    </item>
    <item>
      <title>Re: USB MSD host on TWR-K65F180M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506876#M31828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;J36(2-3) as default&lt;/P&gt;&lt;P&gt;J13(1-1) as default&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Control PTD8 to '1' in code when needed to supply power to the USB output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jan 2016 14:20:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506876#M31828</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2016-01-22T14:20:22Z</dc:date>
    </item>
    <item>
      <title>Re: USB MSD host on TWR-K65F180M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506877#M31829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not entirely sure what the version of the board is; on the back it says 700-28036 REV A, SCH-28036 REV D, (c) 2015 Freescale.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok, it looks like usb_host_board_init sets PTD8. However, it only does so for EHCI (high speed), and I was using KHCI (full speed).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_macro_code _jivemacro_uid_1453760572629637 jive_text_macro" data-renderedposition="92_8_1232_320" jivemacro_uid="_1453760572629637"&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*"0" stands for USB_CONTROLLER_KHCI_0 */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (0 == controller_id)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*"2" stands for USB_CONTROLLER_EHCI_0 */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else if (2 ==controller_id)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*configure the id pin */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enable clock gating to all ports E*/&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CLOCK_SYS_EnablePortClock(4);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTE,10UL,kPortMuxAlt7);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetPullMode(PORTE,10UL,kPortPullUp);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetPullCmd(PORTE,10UL,true);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Source the Ubus. Set PTD8 to high */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enable clock gating to all ports D*/&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CLOCK_SYS_EnablePortClock(3);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIO_DRV_Init(NULL, usbvbushostenablePin);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIO_DRV_WritePinOutput(kGpioUsbVbus, 1);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; else&lt;/P&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once I started using USB_CONTROLLER_EHCI_0, it turns on the USB power and works correctly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jan 2016 21:28:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506877#M31829</guid>
      <dc:creator>acampbell</dc:creator>
      <dc:date>2016-01-26T21:28:40Z</dc:date>
    </item>
    <item>
      <title>Re: USB MSD host on TWR-K65F180M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506878#M31830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Note that the 'readme' file included with the example project usb_host_msd_fatfs (as generated by SDK 2.0) is INCORRECT, at least for USB-HS. It lists incorrect jumper settings. I changed the jumpers to what was stated in the readme file ("J13 1-2, J9 7-8, Remove all jumpers from J23.") and could not even start a debug session. So, keep the jumpers as default:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE border="1" cellpadding="0" cellspacing="0" style="border: none; padding: 0 5.4pt 0 5.4pt;"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD style="border: solid windowtext 1.0pt; padding: 0 5.4pt 0 5.4pt;" valign="top" width="79"&gt;&lt;P style="margin-bottom: .0001pt;"&gt;J13&lt;/P&gt;&lt;/TD&gt;&lt;TD style="border: solid windowtext 1.0pt; border-left: none; padding: 0 5.4pt 0 5.4pt;" valign="top" width="72"&gt;&lt;P style="margin-bottom: .0001pt;"&gt;1-2&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style="border: solid windowtext 1.0pt; border-top: none; padding: 0 5.4pt 0 5.4pt;" valign="top" width="79"&gt;&lt;P style="margin-bottom: .0001pt;"&gt;J9&lt;/P&gt;&lt;/TD&gt;&lt;TD style="border-top: none; border-left: none; border-bottom: solid windowtext 1.0pt; border-right: solid windowtext 1.0pt; padding: 0 5.4pt 0 5.4pt;" valign="top" width="72"&gt;&lt;P style="margin-bottom: .0001pt;"&gt;5-6&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style="border: solid windowtext 1.0pt; border-top: none; padding: 0 5.4pt 0 5.4pt;" valign="top" width="79"&gt;&lt;P style="margin-bottom: .0001pt;"&gt;J23&lt;/P&gt;&lt;/TD&gt;&lt;TD style="border-top: none; border-left: none; border-bottom: solid windowtext 1.0pt; border-right: solid windowtext 1.0pt; padding: 0 5.4pt 0 5.4pt;" valign="top" width="72"&gt;&lt;P style="margin-bottom: .0001pt;"&gt;1-2 &amp;amp; 3-4&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD style="border: solid windowtext 1.0pt; border-top: none; padding: 0 5.4pt 0 5.4pt;" valign="top" width="79"&gt;&lt;P style="margin-bottom: .0001pt;"&gt;J36&lt;/P&gt;&lt;/TD&gt;&lt;TD style="border-top: none; border-left: none; border-bottom: solid windowtext 1.0pt; border-right: solid windowtext 1.0pt; padding: 0 5.4pt 0 5.4pt;" valign="top" width="72"&gt;&lt;P style="margin-bottom: .0001pt;"&gt;2-3&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;And in the code you need to explicitly disable the KHCI build and enable the EHCI build, this is done in usb_host_config.h.&lt;/P&gt;&lt;P&gt;As for the earlier reply, I could not find the function usb_host_dev_mng_check_configuration().&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2016 20:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506878#M31830</guid>
      <dc:creator>paulb-sct</dc:creator>
      <dc:date>2016-02-23T20:43:24Z</dc:date>
    </item>
    <item>
      <title>Re: USB MSD host on TWR-K65F180M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506879#M31831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had this issue to, I assume that debug session is halted because when disconnecting all J23 jumpers (regulator inputs) the USB regulator output voltage is not provided. J9 7-8 source the regulator output to MCU. So with this connection scheme there is no power for MCU!. You can connect J23 1-2 or 3-4 and J9 7-8 when you want to power the mcu only from USB and not from external sources.&lt;BR /&gt;And at last I'm sorry for the wrong function name. That applies for SDK 1.0. For SDK 2.0 it may be equivalent if a function USB_HostInit return success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Lenka Polaskova&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Feb 2016 08:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MSD-host-on-TWR-K65F180M/m-p/506879#M31831</guid>
      <dc:creator>lepol</dc:creator>
      <dc:date>2016-02-25T08:09:42Z</dc:date>
    </item>
  </channel>
</rss>