<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Transmit Complete Flag in Freescale Kinetis USB Stack 4.1.1</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Transmit-Complete-Flag-in-Freescale-Kinetis-USB-Stack-4-1-1/m-p/506850#M31822</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP provides the &lt;A href="http://www.nxp.com/products/software-and-tools/run-time-software/kinetis-software-and-tools/development-platforms-with-mbed/software-development-kit-for-kinetis-mcus:KINETIS-SDK?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;KSDK V2.0 software&lt;/A&gt;, which includes USB Stack for K64 product.&lt;/P&gt;&lt;P&gt;And there also with U&lt;A href="http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/8-bit-s08-5.5v-mcus/usb-stack:MEDICALUSB?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;SB Stack V5.0&lt;/A&gt; for K64 product.&lt;/P&gt;&lt;P&gt;I checked the USB Stack V5.0 CDC device demo, which call USB_Class_CDC_Send_Data() function to transmit 64 bytes data.&lt;/P&gt;&lt;P&gt;Customer could set flag variable at Virtual_Com_App() function of &amp;lt;virtual_com.c&amp;gt; file to check if the data was transmitted.&lt;/P&gt;&lt;P&gt;Customer could check detailed application code info at default path:&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_BM_USB_Stack_v5.0\Src\example\device\cdc\virtual_com\bm\iar\dev_cdc_virtual_com_frdmk64f&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Feb 2016 05:57:05 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2016-02-16T05:57:05Z</dc:date>
    <item>
      <title>Transmit Complete Flag in Freescale Kinetis USB Stack 4.1.1</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Transmit-Complete-Flag-in-Freescale-Kinetis-USB-Stack-4-1-1/m-p/506849#M31821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm using Kinetis K64 MCU with Freescale USB Stack 4.1.1 (CDC).&lt;/P&gt;&lt;P&gt;My application need some flag from USB stack which shows that the data i submitted have sent completely.&lt;/P&gt;&lt;P&gt;Actually i have a queue for data needed to be sent (packet by packet) and with good speed efficiency, i need sent confirmation flag so that i can submit next data to stack for sending.&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Punit Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Feb 2016 13:24:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Transmit-Complete-Flag-in-Freescale-Kinetis-USB-Stack-4-1-1/m-p/506849#M31821</guid>
      <dc:creator>punitkumar</dc:creator>
      <dc:date>2016-02-12T13:24:58Z</dc:date>
    </item>
    <item>
      <title>Re: Transmit Complete Flag in Freescale Kinetis USB Stack 4.1.1</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Transmit-Complete-Flag-in-Freescale-Kinetis-USB-Stack-4-1-1/m-p/506850#M31822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP provides the &lt;A href="http://www.nxp.com/products/software-and-tools/run-time-software/kinetis-software-and-tools/development-platforms-with-mbed/software-development-kit-for-kinetis-mcus:KINETIS-SDK?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;KSDK V2.0 software&lt;/A&gt;, which includes USB Stack for K64 product.&lt;/P&gt;&lt;P&gt;And there also with U&lt;A href="http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/8-bit-s08-5.5v-mcus/usb-stack:MEDICALUSB?fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;SB Stack V5.0&lt;/A&gt; for K64 product.&lt;/P&gt;&lt;P&gt;I checked the USB Stack V5.0 CDC device demo, which call USB_Class_CDC_Send_Data() function to transmit 64 bytes data.&lt;/P&gt;&lt;P&gt;Customer could set flag variable at Virtual_Com_App() function of &amp;lt;virtual_com.c&amp;gt; file to check if the data was transmitted.&lt;/P&gt;&lt;P&gt;Customer could check detailed application code info at default path:&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_BM_USB_Stack_v5.0\Src\example\device\cdc\virtual_com\bm\iar\dev_cdc_virtual_com_frdmk64f&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Feb 2016 05:57:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Transmit-Complete-Flag-in-Freescale-Kinetis-USB-Stack-4-1-1/m-p/506850#M31822</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2016-02-16T05:57:05Z</dc:date>
    </item>
  </channel>
</rss>