<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Setting baud rate to 300bd</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-baud-rate-to-300bd/m-p/506441#M31779</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you are correct !&amp;nbsp; The full baud rate aree supported but not for all system frequency. Customer can use PE to config the BD with different clock frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Fang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Jan 2016 09:07:35 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2016-01-27T09:07:35Z</dc:date>
    <item>
      <title>Setting baud rate to 300bd</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-baud-rate-to-300bd/m-p/506439#M31777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have a problem setting the desired baud rate on my FRDM-K64F board, which is connected to my PC via USB/Serial and runs a simple demo application, sending text messages to a putty client on the PC. Everything works as expected (for many different baud rates, e.g. 9600 bd) until I set the baud rate to 300 bd. With this setting only garbage appears in putty (600 bd is OK btw). So I'm wondering whether 300 bd is just not supported by the device? (I also tried running the board with a system clock of 4MHz and 20Mhz)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jan 2016 18:42:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-baud-rate-to-300bd/m-p/506439#M31777</guid>
      <dc:creator>friedl</dc:creator>
      <dc:date>2016-01-21T18:42:06Z</dc:date>
    </item>
    <item>
      <title>Re: Setting baud rate to 300bd</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-baud-rate-to-300bd/m-p/506440#M31778</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The FRDM-K64F board in principle supports 300bd, but not for all settings of the system clock frequency; e.g., at 120MHz a baud rate of 300bd cannot be set. See baud rate calculation in the reference manual.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jan 2016 20:39:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-baud-rate-to-300bd/m-p/506440#M31778</guid>
      <dc:creator>friedl</dc:creator>
      <dc:date>2016-01-25T20:39:12Z</dc:date>
    </item>
    <item>
      <title>Re: Setting baud rate to 300bd</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-baud-rate-to-300bd/m-p/506441#M31779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you are correct !&amp;nbsp; The full baud rate aree supported but not for all system frequency. Customer can use PE to config the BD with different clock frequency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Fang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jan 2016 09:07:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-baud-rate-to-300bd/m-p/506441#M31779</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-01-27T09:07:35Z</dc:date>
    </item>
  </channel>
</rss>