<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 [K20D50M]: Is USB Device D+ High in VLPS Mode?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20D50M-Is-USB-Device-D-High-in-VLPS-Mode/m-p/503827#M31626</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question regarding D+ status when K20D50 is in VLPS low power mode:&lt;/P&gt;&lt;P&gt;is it still high when K20 enters stop mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jan 2016 06:10:22 GMT</pubDate>
    <dc:creator>huishao2</dc:creator>
    <dc:date>2016-01-20T06:10:22Z</dc:date>
    <item>
      <title>[K20D50M]: Is USB Device D+ High in VLPS Mode?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20D50M-Is-USB-Device-D-High-in-VLPS-Mode/m-p/503827#M31626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question regarding D+ status when K20D50 is in VLPS low power mode:&lt;/P&gt;&lt;P&gt;is it still high when K20 enters stop mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 06:10:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20D50M-Is-USB-Device-D-High-in-VLPS-Mode/m-p/503827#M31626</guid>
      <dc:creator>huishao2</dc:creator>
      <dc:date>2016-01-20T06:10:22Z</dc:date>
    </item>
    <item>
      <title>Re: [K20D50M]: Is USB Device D+ High in VLPS Mode?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20D50M-Is-USB-Device-D-High-in-VLPS-Mode/m-p/503828#M31627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hui,&lt;/P&gt;&lt;P&gt;According to the reference manual, when the USBOTG module enter the low-power mode, its status will move to the Suspend mode.&lt;/P&gt;&lt;P&gt;While in the Suspend state, a device must continue to provide power to its D+ ( full/high-speed ) or D- ( low-speed ) pull up resistor to maintain an idle so that the upstream hub can maintain the correct connectivity status for the device.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jan 2016 02:50:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K20D50M-Is-USB-Device-D-High-in-VLPS-Mode/m-p/503828#M31627</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-01-21T02:50:40Z</dc:date>
    </item>
  </channel>
</rss>