<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: FTM Fault Detection Inputs in KV31</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Fault-Detection-Inputs-in-KV31/m-p/503822#M31625</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sören,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suppose that both chapters are correct, because in SIM_SOPT4 register you can choose fault detection input between two possible options (fault pin or CMP), for example FTM1_FAULT0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even, FTM1_FAULT1 is hardwired to CMP1 output, thus, you are not able to change Fault input. There is not required changes in register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;M.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Apr 2016 15:08:04 GMT</pubDate>
    <dc:creator>marekzeman-b508</dc:creator>
    <dc:date>2016-04-14T15:08:04Z</dc:date>
    <item>
      <title>FTM Fault Detection Inputs in KV31</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Fault-Detection-Inputs-in-KV31/m-p/503821#M31624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ChipConfigurationFTMFaults.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32101i878FE18B57B0B4BE/image-size/large?v=v2&amp;amp;px=999" role="button" title="ChipConfigurationFTMFaults.PNG" alt="ChipConfigurationFTMFaults.PNG" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="SIMSOPT_Bits.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32201i966364BC3AC77397/image-size/large?v=v2&amp;amp;px=999" role="button" title="SIMSOPT_Bits.PNG" alt="SIMSOPT_Bits.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hey there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have a&amp;nbsp; question about FTM Fault in MKV31F512VLL12 reference manual. As depicted above the chip configuration chapter has more fault detection input than the SIM_SOPT4 has bits for. Which one is correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sören&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Apr 2016 09:01:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Fault-Detection-Inputs-in-KV31/m-p/503821#M31624</guid>
      <dc:creator>soerenbirth</dc:creator>
      <dc:date>2016-04-14T09:01:49Z</dc:date>
    </item>
    <item>
      <title>Re: FTM Fault Detection Inputs in KV31</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Fault-Detection-Inputs-in-KV31/m-p/503822#M31625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sören,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suppose that both chapters are correct, because in SIM_SOPT4 register you can choose fault detection input between two possible options (fault pin or CMP), for example FTM1_FAULT0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even, FTM1_FAULT1 is hardwired to CMP1 output, thus, you are not able to change Fault input. There is not required changes in register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;M.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Apr 2016 15:08:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FTM-Fault-Detection-Inputs-in-KV31/m-p/503822#M31625</guid>
      <dc:creator>marekzeman-b508</dc:creator>
      <dc:date>2016-04-14T15:08:04Z</dc:date>
    </item>
  </channel>
</rss>