<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: eDMA with different source/destination data sizes</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/eDMA-with-different-source-destination-data-sizes/m-p/503476#M31594</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jason,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the eDMA can do the padding automatically, the source data transfer size can be different than the destination data transfer size (please take a look into the &lt;STRONG&gt;DMA_TDCn_ATTR[SSIZE]&lt;/STRONG&gt; and &lt;STRONG&gt;DMA_TDCn_ATTR[DSIZE]&lt;/STRONG&gt; register fields).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this answer your question? If it doesn't please don't hesitate in contact me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jan 2016 18:27:09 GMT</pubDate>
    <dc:creator>EarlOrlando</dc:creator>
    <dc:date>2016-01-20T18:27:09Z</dc:date>
    <item>
      <title>eDMA with different source/destination data sizes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/eDMA-with-different-source-destination-data-sizes/m-p/503475#M31593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an application that requires a TDM8 stream to be transmitted using the I2S/SAI module. Said stream consists of eight channels of 16-bit audio. The receiver requires each TDM frame to be 32 bytes, or 256 bits, in length regardless of the actual data size. Using MSB-first transmission, each frame should begin with the MSB-LSB of the first channel, followed by 16 empty bits, then the MSB-LSB of the second channel, another 16 empty bits, and so on. To conserve memory, the source buffer within the Kinetis is an array of int16_t, so there is no padding between channels. Is it possible to configure the eDMA to read 16-bit data from the source, and write 32-bit data to the I2S TX FIFO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Jason Valenzuela&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 05:41:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/eDMA-with-different-source-destination-data-sizes/m-p/503475#M31593</guid>
      <dc:creator>jvalenzuela</dc:creator>
      <dc:date>2016-01-20T05:41:31Z</dc:date>
    </item>
    <item>
      <title>Re: eDMA with different source/destination data sizes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/eDMA-with-different-source-destination-data-sizes/m-p/503476#M31594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jason,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the eDMA can do the padding automatically, the source data transfer size can be different than the destination data transfer size (please take a look into the &lt;STRONG&gt;DMA_TDCn_ATTR[SSIZE]&lt;/STRONG&gt; and &lt;STRONG&gt;DMA_TDCn_ATTR[DSIZE]&lt;/STRONG&gt; register fields).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this answer your question? If it doesn't please don't hesitate in contact me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 18:27:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/eDMA-with-different-source-destination-data-sizes/m-p/503476#M31594</guid>
      <dc:creator>EarlOrlando</dc:creator>
      <dc:date>2016-01-20T18:27:09Z</dc:date>
    </item>
  </channel>
</rss>