<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Could I replace the MK22FN512VLH12 on the Freedom Board (FRDM-K22F) with a MK22FN1M0AVLH12? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Could-I-replace-the-MK22FN512VLH12-on-the-Freedom-Board-FRDM/m-p/502096#M31458</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I replace the MK22FN512VLH12 on the Freedom Board (FRDM-K22F) with a MK22FN1M0AVLH12, from the same k22f family, would I be able to use all the features of the MK22FN1M0AVLH12? I'm talking about CAN, I2C, SPI, and so on.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 May 2016 18:31:54 GMT</pubDate>
    <dc:creator>brentgreenwald</dc:creator>
    <dc:date>2016-05-25T18:31:54Z</dc:date>
    <item>
      <title>Could I replace the MK22FN512VLH12 on the Freedom Board (FRDM-K22F) with a MK22FN1M0AVLH12?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Could-I-replace-the-MK22FN512VLH12-on-the-Freedom-Board-FRDM/m-p/502096#M31458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I replace the MK22FN512VLH12 on the Freedom Board (FRDM-K22F) with a MK22FN1M0AVLH12, from the same k22f family, would I be able to use all the features of the MK22FN1M0AVLH12? I'm talking about CAN, I2C, SPI, and so on.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 May 2016 18:31:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Could-I-replace-the-MK22FN512VLH12-on-the-Freedom-Board-FRDM/m-p/502096#M31458</guid>
      <dc:creator>brentgreenwald</dc:creator>
      <dc:date>2016-05-25T18:31:54Z</dc:date>
    </item>
    <item>
      <title>Re: Could I replace the MK22FN512VLH12 on the Freedom Board (FRDM-K22F) with a MK22FN1M0AVLH12?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Could-I-replace-the-MK22FN512VLH12-on-the-Freedom-Board-FRDM/m-p/502097#M31459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brent Greenwald&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the Pinout position and it matched, regardless, It is NOT recommendable to do this, there are some modules available in MK22FN1M0AVLH12 that there aren't in MK22FN512VLH12. You can check the following link that describe this differences: &lt;A href="https://community.nxp.com/docs/DOC-102548"&gt;Kinetis K22_120 MHz devices &lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The official Board for MK22FN1M0AVLH12 is the TWR-K21F120MA. You could consider to use it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 May 2016 23:34:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Could-I-replace-the-MK22FN512VLH12-on-the-Freedom-Board-FRDM/m-p/502097#M31459</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2016-05-26T23:34:42Z</dc:date>
    </item>
  </channel>
</rss>