<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KL16 or KL26 SPI DMA example with processor expert in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16-or-KL26-SPI-DMA-example-with-processor-expert/m-p/501923#M31439</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you would like to stick to processor expert code or you can also do with bare-metal code like Kinetis SDK?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to use processor expert code, then you can choose KDS IDE from &lt;A href="https://community.nxp.com/www.nxp.com/kds" target="test_blank"&gt;www.nxp.com/kds&lt;/A&gt;, create a processor expert project for KL26, then drag and drop a SPI_LDD component for KL26.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or you can choose to download Kinetis SDK code from &lt;A href="https://community.nxp.com/www.nxp.com/ksdk" target="test_blank"&gt;www.nxp.com/ksdk&lt;/A&gt;, there is example code for SPI DMA in the KSDK1.3 package for KL26 Freedom board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56153i60C9383F1B49BACE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Mar 2016 13:42:49 GMT</pubDate>
    <dc:creator>cutworth</dc:creator>
    <dc:date>2016-03-02T13:42:49Z</dc:date>
    <item>
      <title>KL16 or KL26 SPI DMA example with processor expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16-or-KL26-SPI-DMA-example-with-processor-expert/m-p/501922#M31438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello,&lt;/P&gt;&lt;P&gt;I try to use small OLED display (92x64px) with SPI but the bus is slow. I can't find any example with SPI and DMA on KL16 or KL26 MCU. Is there any sample code with this combination? I found DMA with UART or ADC but not with SPI. Thanks for any help.&lt;/P&gt;&lt;P&gt;Michal.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Mar 2016 13:11:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16-or-KL26-SPI-DMA-example-with-processor-expert/m-p/501922#M31438</guid>
      <dc:creator>misiek81_pl</dc:creator>
      <dc:date>2016-03-02T13:11:30Z</dc:date>
    </item>
    <item>
      <title>Re: KL16 or KL26 SPI DMA example with processor expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16-or-KL26-SPI-DMA-example-with-processor-expert/m-p/501923#M31439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you would like to stick to processor expert code or you can also do with bare-metal code like Kinetis SDK?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to use processor expert code, then you can choose KDS IDE from &lt;A href="https://community.nxp.com/www.nxp.com/kds" target="test_blank"&gt;www.nxp.com/kds&lt;/A&gt;, create a processor expert project for KL26, then drag and drop a SPI_LDD component for KL26.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or you can choose to download Kinetis SDK code from &lt;A href="https://community.nxp.com/www.nxp.com/ksdk" target="test_blank"&gt;www.nxp.com/ksdk&lt;/A&gt;, there is example code for SPI DMA in the KSDK1.3 package for KL26 Freedom board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/56153i60C9383F1B49BACE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Mar 2016 13:42:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL16-or-KL26-SPI-DMA-example-with-processor-expert/m-p/501923#M31439</guid>
      <dc:creator>cutworth</dc:creator>
      <dc:date>2016-03-02T13:42:49Z</dc:date>
    </item>
  </channel>
</rss>