<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Difference flash memory secure / unsecure mode KEA128 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Difference-flash-memory-secure-unsecure-mode-KEA128/m-p/501796#M31423</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Actually the table 18-4 is correct that all flash commands are available in both states. The true difference between the secure and un-secured mode is for debug port. That is to say the flash commands are always available for MCU core, but is not available for access through debug interface when in secure mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Mar 2016 06:00:55 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2016-03-07T06:00:55Z</dc:date>
    <item>
      <title>Difference flash memory secure / unsecure mode KEA128</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Difference-flash-memory-secure-unsecure-mode-KEA128/m-p/501795#M31422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I am trying to setup a bootloader on a S9KEAZ128 chip that enables software updating, and was reading into the flash protection mechanisms. I noticed on page 249-250 of the reference manual that the flash module FTMRE can either be secured or unsecured, but table 18-4 states all flash command are available in both states. Could it be that the table is incorrect?&lt;/P&gt;&lt;P&gt;I am trying to understand what the practical difference between these two states is, and how to use them.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Mar 2016 08:44:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Difference-flash-memory-secure-unsecure-mode-KEA128/m-p/501795#M31422</guid>
      <dc:creator>joopaandentoorn</dc:creator>
      <dc:date>2016-03-02T08:44:48Z</dc:date>
    </item>
    <item>
      <title>Re: Difference flash memory secure / unsecure mode KEA128</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Difference-flash-memory-secure-unsecure-mode-KEA128/m-p/501796#M31423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Actually the table 18-4 is correct that all flash commands are available in both states. The true difference between the secure and un-secured mode is for debug port. That is to say the flash commands are always available for MCU core, but is not available for access through debug interface when in secure mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Mar 2016 06:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Difference-flash-memory-secure-unsecure-mode-KEA128/m-p/501796#M31423</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2016-03-07T06:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: Difference flash memory secure / unsecure mode KEA128</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Difference-flash-memory-secure-unsecure-mode-KEA128/m-p/501797#M31424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah that makes sense. Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Mar 2016 08:26:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Difference-flash-memory-secure-unsecure-mode-KEA128/m-p/501797#M31424</guid>
      <dc:creator>joopaandentoorn</dc:creator>
      <dc:date>2016-03-07T08:26:14Z</dc:date>
    </item>
  </channel>
</rss>