<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックCodeWarrior support for MK60X256VLQ100</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CodeWarrior-support-for-MK60X256VLQ100/m-p/205013#M3141</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on my first project using CodeWarrior and I have a question regarding support for the Kinetis MK60X256VLQ100, which is the LQFP144 package. When I create the project and select the MK60 family, I only see support for the BGA package when I try to use the Device Initialization tool. I know I must be missing a selection somewhere, but I can't see it. Thanks for any help anyone might be able to provide.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Dec 2012 02:21:34 GMT</pubDate>
    <dc:creator>WadeJones</dc:creator>
    <dc:date>2012-12-12T02:21:34Z</dc:date>
    <item>
      <title>CodeWarrior support for MK60X256VLQ100</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CodeWarrior-support-for-MK60X256VLQ100/m-p/205013#M3141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on my first project using CodeWarrior and I have a question regarding support for the Kinetis MK60X256VLQ100, which is the LQFP144 package. When I create the project and select the MK60 family, I only see support for the BGA package when I try to use the Device Initialization tool. I know I must be missing a selection somewhere, but I can't see it. Thanks for any help anyone might be able to provide.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2012 02:21:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CodeWarrior-support-for-MK60X256VLQ100/m-p/205013#M3141</guid>
      <dc:creator>WadeJones</dc:creator>
      <dc:date>2012-12-12T02:21:34Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior support for MK60X256VLQ100</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CodeWarrior-support-for-MK60X256VLQ100/m-p/205014#M3142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Once you create the project selecting the processor variant (MK60DX256 / MK60DX256Z) and the Device Initialization tool, go to the Target CPU tab, and click on Select CPU package, a small window will pop up showing you the available packages, select MK60DX256VLQ10 (144 LQFP) and you're right on track.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Dec 2012 17:21:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CodeWarrior-support-for-MK60X256VLQ100/m-p/205014#M3142</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2012-12-12T17:21:16Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior support for MK60X256VLQ100</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CodeWarrior-support-for-MK60X256VLQ100/m-p/205015#M3143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That worked. Thanks for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Dec 2012 17:01:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CodeWarrior-support-for-MK60X256VLQ100/m-p/205015#M3143</guid>
      <dc:creator>WadeJones</dc:creator>
      <dc:date>2012-12-13T17:01:20Z</dc:date>
    </item>
  </channel>
</rss>