<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: MKV56F512VLL20</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV56F512VLL20/m-p/500672#M31312</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erskine,&lt;/P&gt;&lt;P&gt;I've attached the startup and liker files of the KV31 instead of the KV56 , and you can port these files to the KV56 easily.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 May 2016 03:11:53 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2016-05-05T03:11:53Z</dc:date>
    <item>
      <title>MKV56F512VLL20</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV56F512VLL20/m-p/500671#M31311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anyone please post a link for initialization code for a MKV56F512VLL20? It is not listed in Processor Expert.&amp;nbsp; A project that can be imported into IAR would be great. I have found several locations on the Freescale Website that indicated its presents, but nothing there. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 May 2016 13:08:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV56F512VLL20/m-p/500671#M31311</guid>
      <dc:creator>erskineb</dc:creator>
      <dc:date>2016-05-04T13:08:34Z</dc:date>
    </item>
    <item>
      <title>Re: MKV56F512VLL20</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV56F512VLL20/m-p/500672#M31312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erskine,&lt;/P&gt;&lt;P&gt;I've attached the startup and liker files of the KV31 instead of the KV56 , and you can port these files to the KV56 easily.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 May 2016 03:11:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKV56F512VLL20/m-p/500672#M31312</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-05-05T03:11:53Z</dc:date>
    </item>
  </channel>
</rss>