<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Using UART with RS485 on K64F microcontroller</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500623#M31306</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Magical :smileywink: &lt;/P&gt;&lt;P&gt;Thats &lt;SPAN style="text-decoration: underline;"&gt;exactly&lt;/SPAN&gt; the info I needed. I wanted to be sure that I have to add a transceiver to the uart rx tx rts myself or if there is one obscure rs485 channel integrated into the module, you know, because of convenience or something.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will set the TXRTSE bit (automatic flow control) in the correct uart modem register and set the polarity of the RTS signal to the required polarity of my transceiver and then it should work, right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I can get on with my life, thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 May 2016 16:24:33 GMT</pubDate>
    <dc:creator>michaelkoller</dc:creator>
    <dc:date>2016-05-09T16:24:33Z</dc:date>
    <item>
      <title>Using UART with RS485 on K64F microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500617#M31300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I have to communicate with a motor driver that has a RS485 type physical interface and a given command format. I am now trying to communicate with it via UART on the K64F but the manual (the one with over 1500 pages) has very little information about it. Are there any sources I can look up?&lt;/P&gt;&lt;P&gt;Anything helps, thanks in advance and&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 May 2016 14:48:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500617#M31300</guid>
      <dc:creator>michaelkoller</dc:creator>
      <dc:date>2016-05-05T14:48:51Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART with RS485 on K64F microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500618#M31301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael Koller&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP provides RS485 example code for K20 product based on MQX RTOS.&lt;/P&gt;&lt;P&gt;Please check the default path (C:\Freescale\Freescale_MQX_4_X\mqx\examples\rs485) to find that example.&lt;/P&gt;&lt;P&gt;NXP MQX could be download &lt;A class="jive-link-external-small" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freescale.com%2Fwebapp%2Fsps%2Fsite%2Fprod_summary.jsp%3Fcode%3DMQX" rel="nofollow" target="_blank"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 May 2016 19:19:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500618#M31301</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2016-05-06T19:19:00Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART with RS485 on K64F microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500619#M31302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;Thank you for the answer, but I don't really understand how I should use this information, probably because I'm too inexperienced. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the K64F and not something from the K20 product line.&lt;/P&gt;&lt;P&gt;Do you mean that I can include the right header from the K20 MQX RTOS files in my current K64F project and the correct code from the example project in my main.c?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Optimally, I would like to have some code, that transforms my tx and rx pins (c16 and c17are broken out on the K64F devboard, so I use that) into the rs485+ and rs485- differential signal pins. These pins I could then connect to the the rs485 interface from the driver, which I want to communicate with.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this achieveable with the link you sent me (and what's the best way to set it up, then)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for the pointer in the hopefully right direction, maybe you can elaborate a little bit more!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 May 2016 17:32:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500619#M31302</guid>
      <dc:creator>michaelkoller</dc:creator>
      <dc:date>2016-05-07T17:32:42Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART with RS485 on K64F microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500620#M31303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also, I don't use Processor Expert or anything like it. I need solutions, that I can implement vie C++ code myself. Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit: I should mention that I use Ubuntu. So in order to install it I followed the Getting Started PDF &lt;A href="http://www.nxp.com/products/software-and-tools/run-time-software/nxp-mqx-software-solutions/mqx-real-time-operating-system-rtos/mqx-classic-software-solutions:MQX?code=MQX&amp;amp;nodeId=0152109D3F60795BB6&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab" title="http://www.nxp.com/products/software-and-tools/run-time-software/nxp-mqx-software-solutions/mqx-real-time-operating-system-rtos/mqx-classic-software-solutions:MQX?code=MQX&amp;amp;nodeId=0152109D3F60795BB6&amp;amp;fpsp=1&amp;amp;tab=Documentation_Tab"&gt;MQX™ Classic Software Solutions|NXP&lt;/A&gt;&amp;nbsp; There it says to look up the&lt;/P&gt;&lt;P&gt;Getting Started with Kinetis Design Studio IDE and Freescale MQXTM RTOS.pdf in the unpacked Download for MQX, which I did.&lt;/P&gt;&lt;P&gt;There it tells me to follow the steps where I need to go to Help-&amp;gt; Install New Software --&amp;gt; got to Freescale Update Site --&amp;gt; check MQX Installations --&amp;gt; proceed with installation.&lt;/P&gt;&lt;P&gt;I find do that and it gives me this error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;An error occurred while collecting items to be installed&lt;/P&gt;&lt;P&gt;session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).&lt;/P&gt;&lt;P&gt;No repository found containing: osgi.bundle,com.freescale.dom4j.lib,1.1.1.201508111009&lt;/P&gt;&lt;P&gt;No repository found containing: osgi.bundle,com.freescale.mqx.gdb.tad,1.0.9.201508111009&lt;/P&gt;&lt;P&gt;No repository found containing: org.eclipse.update.feature,com.freescale.mqx.gdb.tad.eclipse,1.0.9.201508111009&lt;/P&gt;&lt;P&gt;No repository found containing: osgi.bundle,com.freescale.mqx.projectofprojects,1.1.8.201508111009&lt;/P&gt;&lt;P&gt;No repository found containing: org.eclipse.update.feature,com.freescale.mqx.projectofprojects.eclipse,1.1.8.201508111009&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the problem?&lt;/P&gt;&lt;P&gt;I appreciate any guidance,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit: Another question: Am I correct to assume that with this MQX I won't need additional hardware for rs485? I would like not to have to use a transceiver.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 May 2016 17:59:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500620#M31303</guid>
      <dc:creator>michaelkoller</dc:creator>
      <dc:date>2016-05-07T17:59:37Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART with RS485 on K64F microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500621#M31304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no magical software to turn the UART TX and RX pins output into RS485. RS485 is an electrical specification. You will have to add electrical components to the UART TX/RX circuit to convert it to RS485. The UART can talk on a RS485 circuit if the proper electrical components are added.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your UART code will then need to be modified to deal with RS485 transmitted data looping back in the RX/TX circuit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 May 2016 15:38:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500621#M31304</guid>
      <dc:creator>ndavies</dc:creator>
      <dc:date>2016-05-09T15:38:12Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART with RS485 on K64F microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500622#M31305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael Koller&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I’m sorry if my response cause confusion. &lt;SPAN class="shorttext"&gt;Unfortunately we don’t have an example code of RS485 in bareboard, there is only an example code using RTOS, and for this, it is necessary install MQX, and then you can look at the path that I mentioned. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="shorttext"&gt;This example code is design to be used with the TWR of NXP, in this case, the twr64f120m, and it’s necessary used the twr-ser1 or twr-ser2.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="shorttext"&gt;It is possible that you let us know the version of MQX that you’re installing?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="shorttext"&gt;&lt;SPAN class="shorttext"&gt;Attached is the "readme" file for the RS485 example&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 May 2016 15:54:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500622#M31305</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2016-05-09T15:54:50Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART with RS485 on K64F microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500623#M31306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Magical :smileywink: &lt;/P&gt;&lt;P&gt;Thats &lt;SPAN style="text-decoration: underline;"&gt;exactly&lt;/SPAN&gt; the info I needed. I wanted to be sure that I have to add a transceiver to the uart rx tx rts myself or if there is one obscure rs485 channel integrated into the module, you know, because of convenience or something.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will set the TXRTSE bit (automatic flow control) in the correct uart modem register and set the polarity of the RTS signal to the required polarity of my transceiver and then it should work, right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I can get on with my life, thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 May 2016 16:24:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-UART-with-RS485-on-K64F-microcontroller/m-p/500623#M31306</guid>
      <dc:creator>michaelkoller</dc:creator>
      <dc:date>2016-05-09T16:24:33Z</dc:date>
    </item>
  </channel>
</rss>