<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UART send break in K60. in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-send-break-in-K60/m-p/499930#M31216</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Albert:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the time with no responses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you still having this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Typically the BREAK character is formed by logic 0s, ¿so are you using the TX inverted mode? In that case you would need to just leave the line idle for the required 8.33 ms to get the 0 logic mark you are expecting, or force an idle character by clearing and setting C2[TE] as explained in the manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58433i9D1EA38D698636E6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Mar 2016 22:11:25 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2016-03-07T22:11:25Z</dc:date>
    <item>
      <title>UART send break in K60.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-send-break-in-K60/m-p/499928#M31214</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to implement the SDI-12 Master (&lt;A href="http://www.sdi-12.org/" title="http://www.sdi-12.org/"&gt;SDI-12 Support Group&lt;/A&gt; )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can configure properly the UART for transmission data:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;1200 bps (Baudrate), 7 bit, even parity with 1 stop bit and 1 start bit.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I don't know how can i SEND break and mask.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Idea is :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27857iEC3A76E1035F3456/image-size/large?v=v2&amp;amp;px=999" title="Sin título.png" alt="Sin título.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The beak is aprox 14 bits to high level&lt;/P&gt;&lt;P&gt;The mark is 10 bits to low level.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can find this charapter into K60P144M150SF3RM document.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;55.4.2.4 Transmitting break characters&lt;/LI&gt;&lt;LI&gt;55.4.2.5 Idle characters&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, i don't udenderd how can i do it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks you very much for everything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Albert.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Feb 2016 09:18:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-send-break-in-K60/m-p/499928#M31214</guid>
      <dc:creator>albert1199</dc:creator>
      <dc:date>2016-02-10T09:18:28Z</dc:date>
    </item>
    <item>
      <title>Re: UART send break in K60.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-send-break-in-K60/m-p/499929#M31215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can find a part of solution:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; UART1-&amp;gt;C2 |= UART_C2_TE_MASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; UART1-&amp;gt;C2 |= UART_C2_SBK_MASK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; UART1-&amp;gt;C2 &amp;amp;=&amp;nbsp; (uint8_t)(~(uint8_t)UART_C2_SBK_MASK);&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With this solution, i can transmit one break characters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But in this case, I only get the break. It is logic 1 part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35687i1E50700D96699F81/image-size/large?v=v2&amp;amp;px=999" title="TEK00000.PNG" alt="TEK00000.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;know how i can find the mark (8.33 ms set 0 logic).??&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Thanks you very much.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Feb 2016 16:59:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-send-break-in-K60/m-p/499929#M31215</guid>
      <dc:creator>albert1199</dc:creator>
      <dc:date>2016-02-11T16:59:52Z</dc:date>
    </item>
    <item>
      <title>Re: UART send break in K60.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-send-break-in-K60/m-p/499930#M31216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Albert:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the time with no responses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you still having this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Typically the BREAK character is formed by logic 0s, ¿so are you using the TX inverted mode? In that case you would need to just leave the line idle for the required 8.33 ms to get the 0 logic mark you are expecting, or force an idle character by clearing and setting C2[TE] as explained in the manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58433i9D1EA38D698636E6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Mar 2016 22:11:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-send-break-in-K60/m-p/499930#M31216</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2016-03-07T22:11:25Z</dc:date>
    </item>
  </channel>
</rss>